<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Reset assert time for S12ZNML/S12ZVMBA in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Reset-assert-time-for-S12ZNML-S12ZVMBA/m-p/672809#M14130</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is an internal RC filter which is characterized with the RP_MASK and RP_PASS values. Pulses smaller than 12ns are filtered, pulses greater than 22ns are not filtered. The internal RC filter is subject to some variance so pulses with a length between 12 and 22ns may or may not reset the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you need your own RC filter, make sure that the reset pulse last less then 24us, as the &lt;A href="http://www.nxp.com/assets/documents/data/en/application-notes/AN5207.pdf"&gt;Hardware Design Guidelines for S12ZVM Microcontrollers (AN5207)&lt;/A&gt; explains.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Jun 2017 09:19:02 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2017-06-02T09:19:02Z</dc:date>
    <item>
      <title>Reset assert time for S12ZNML/S12ZVMBA</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Reset-assert-time-for-S12ZNML-S12ZVMBA/m-p/672808#M14129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Want to know the minimum reset assert time on Reset pin for the MCU to execute reset for S12ZVML and S12ZVMBA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basically want to design the correct RC values for reset circuit: any guidelines on this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found some timing values related to Reset pin in the datasheet (attachment photo, highlighted terms), please explain them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Jun 2017 02:28:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Reset-assert-time-for-S12ZNML-S12ZVMBA/m-p/672808#M14129</guid>
      <dc:creator>rajivbandodkar</dc:creator>
      <dc:date>2017-06-02T02:28:11Z</dc:date>
    </item>
    <item>
      <title>Re: Reset assert time for S12ZNML/S12ZVMBA</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Reset-assert-time-for-S12ZNML-S12ZVMBA/m-p/672809#M14130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is an internal RC filter which is characterized with the RP_MASK and RP_PASS values. Pulses smaller than 12ns are filtered, pulses greater than 22ns are not filtered. The internal RC filter is subject to some variance so pulses with a length between 12 and 22ns may or may not reset the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you need your own RC filter, make sure that the reset pulse last less then 24us, as the &lt;A href="http://www.nxp.com/assets/documents/data/en/application-notes/AN5207.pdf"&gt;Hardware Design Guidelines for S12ZVM Microcontrollers (AN5207)&lt;/A&gt; explains.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Jun 2017 09:19:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Reset-assert-time-for-S12ZNML-S12ZVMBA/m-p/672809#M14130</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-06-02T09:19:02Z</dc:date>
    </item>
  </channel>
</rss>