<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 pull up/down recommendation for external data bus of S12</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/pull-up-down-recommendation-for-external-data-bus-of-S12/m-p/671292#M14105</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we are operating a MC9S12XDP512 / MC9S12XEP100 micro controller in expanded mode. On the external bus a static RAM IC is connected without external pull up / down resistors on data bus.&lt;/P&gt;&lt;P&gt;What is your the recommendation regarding pull up / down resistors:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;do we need pull up or pull down at all on the external data bus to have a defined signal level in case the external static RAM IC is not accessed?&lt;/LI&gt;&lt;LI&gt;should / can we make use of the internal pull up feature of PORT C / D to have defined signal levels on the external data bus (set PUPDE PUPCE in PUCR register)?&lt;/LI&gt;&lt;LI&gt;should we better use external pull up / down resistor to have defined signal levels on the external data bus?&lt;/LI&gt;&lt;LI&gt;is there an application note about this topic and where do we find it?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are looking forward to get an answer to the questions soon.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With kind regards&lt;/P&gt;&lt;P&gt;Leopold&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 May 2017 15:13:28 GMT</pubDate>
    <dc:creator>leopoldgemsch</dc:creator>
    <dc:date>2017-05-08T15:13:28Z</dc:date>
    <item>
      <title>pull up/down recommendation for external data bus of S12</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/pull-up-down-recommendation-for-external-data-bus-of-S12/m-p/671292#M14105</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we are operating a MC9S12XDP512 / MC9S12XEP100 micro controller in expanded mode. On the external bus a static RAM IC is connected without external pull up / down resistors on data bus.&lt;/P&gt;&lt;P&gt;What is your the recommendation regarding pull up / down resistors:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;do we need pull up or pull down at all on the external data bus to have a defined signal level in case the external static RAM IC is not accessed?&lt;/LI&gt;&lt;LI&gt;should / can we make use of the internal pull up feature of PORT C / D to have defined signal levels on the external data bus (set PUPDE PUPCE in PUCR register)?&lt;/LI&gt;&lt;LI&gt;should we better use external pull up / down resistor to have defined signal levels on the external data bus?&lt;/LI&gt;&lt;LI&gt;is there an application note about this topic and where do we find it?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are looking forward to get an answer to the questions soon.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With kind regards&lt;/P&gt;&lt;P&gt;Leopold&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 May 2017 15:13:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/pull-up-down-recommendation-for-external-data-bus-of-S12/m-p/671292#M14105</guid>
      <dc:creator>leopoldgemsch</dc:creator>
      <dc:date>2017-05-08T15:13:28Z</dc:date>
    </item>
    <item>
      <title>Re: pull up/down recommendation for external data bus of S12</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/pull-up-down-recommendation-for-external-data-bus-of-S12/m-p/671293#M14106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;a) as a first step I would like to direct you to my supporting material:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-93594"&gt;https://community.nxp.com/docs/DOC-93594&lt;/A&gt; &lt;/P&gt;&lt;P&gt;Please read it carefully. It will simplify your design and debugging issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;b) No there is no reason to have any pull resistor on the bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have any additional questions, do not hesitate to ask....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ladislav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 May 2017 08:33:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/pull-up-down-recommendation-for-external-data-bus-of-S12/m-p/671293#M14106</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2017-05-09T08:33:49Z</dc:date>
    </item>
  </channel>
</rss>