<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: Max Current From Ballast Transistor</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Max-Current-From-Ballast-Transistor/m-p/662967#M13990</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This is not defined, only max current IDDX without the external PNP (see Table E-1 of the RM). If the current exceeds this value, the external PNP is required. BCTL provides the base current of the transistor. The Table E-1 provides minimal base current that can be guaranteed. Then the gain of the transistor controls the maximum available current.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please refer to &lt;A href="http://www.nxp.com/assets/documents/data/en/application-notes/AN4867.pdf"&gt;Hardware Design Guidelines for S12ZVC&lt;/A&gt; for more information.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 10 Apr 2017 21:09:06 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2017-04-10T21:09:06Z</dc:date>
    <item>
      <title>Max Current From Ballast Transistor</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Max-Current-From-Ballast-Transistor/m-p/662966#M13989</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;EM&gt;How much current can the external ballast transistor supply when used in conjunction with the 9S12ZVCA processor BCTL pin?&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 09 Apr 2017 09:59:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Max-Current-From-Ballast-Transistor/m-p/662966#M13989</guid>
      <dc:creator>gordonp</dc:creator>
      <dc:date>2017-04-09T09:59:54Z</dc:date>
    </item>
    <item>
      <title>Re: Max Current From Ballast Transistor</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Max-Current-From-Ballast-Transistor/m-p/662967#M13990</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This is not defined, only max current IDDX without the external PNP (see Table E-1 of the RM). If the current exceeds this value, the external PNP is required. BCTL provides the base current of the transistor. The Table E-1 provides minimal base current that can be guaranteed. Then the gain of the transistor controls the maximum available current.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please refer to &lt;A href="http://www.nxp.com/assets/documents/data/en/application-notes/AN4867.pdf"&gt;Hardware Design Guidelines for S12ZVC&lt;/A&gt; for more information.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Apr 2017 21:09:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Max-Current-From-Ballast-Transistor/m-p/662967#M13990</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-04-10T21:09:06Z</dc:date>
    </item>
  </channel>
</rss>