<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: LS0 Fault of S12VR</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/LS0-Fault-of-S12VR/m-p/656974#M13896</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jason,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Could you please specify what you mean by “the LS0 pin get out of control”?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Do you mean that the code works correctly, but low side switch does not react on LSDR_LSDR0 bit modification? Or code do not react on external request?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is it temporary failure (until MCU reset) or permanent (MCU replacement is necessary)?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Each low-side driver has an over-current detection while enabled with a current threshold of ILIMLSX. If over-current is detected the related interrupt flag (LSOCIF1 or LSOCIF0) is set in the LSDRV Interrupt Flag Register (LSIF). As long as the over-current interrupt flag remains set the related low-side driver is turned off to protect the circuit.Clearing the related over-current interrupt flag returns back the control of the driver to the selected source in the PIM module.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Additionally, there is an active clamp (for driving relays) protecting each driver stage. The active clamp will turn on a low-side FET if the voltage on a pin exceeds VCLAMP (min. 40V) when the driver is turned off.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If possible, please specify also MCU maskset and share schematic for short check for any obvious/potential issue.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Jan 2017 16:39:46 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2017-01-04T16:39:46Z</dc:date>
    <item>
      <title>LS0 Fault of S12VR</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/LS0-Fault-of-S12VR/m-p/656973#M13895</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;There are some product whose LS0 Pin get out of control.We use S12VR for ANTI PINCH,and the LS0 is used to control the Relay.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could tell me what reason may result the LS0 pin get out of control?&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jan 2017 08:52:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/LS0-Fault-of-S12VR/m-p/656973#M13895</guid>
      <dc:creator>jasoncao</dc:creator>
      <dc:date>2017-01-03T08:52:04Z</dc:date>
    </item>
    <item>
      <title>Re: LS0 Fault of S12VR</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/LS0-Fault-of-S12VR/m-p/656974#M13896</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jason,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Could you please specify what you mean by “the LS0 pin get out of control”?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Do you mean that the code works correctly, but low side switch does not react on LSDR_LSDR0 bit modification? Or code do not react on external request?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is it temporary failure (until MCU reset) or permanent (MCU replacement is necessary)?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Each low-side driver has an over-current detection while enabled with a current threshold of ILIMLSX. If over-current is detected the related interrupt flag (LSOCIF1 or LSOCIF0) is set in the LSDRV Interrupt Flag Register (LSIF). As long as the over-current interrupt flag remains set the related low-side driver is turned off to protect the circuit.Clearing the related over-current interrupt flag returns back the control of the driver to the selected source in the PIM module.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Additionally, there is an active clamp (for driving relays) protecting each driver stage. The active clamp will turn on a low-side FET if the voltage on a pin exceeds VCLAMP (min. 40V) when the driver is turned off.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If possible, please specify also MCU maskset and share schematic for short check for any obvious/potential issue.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jan 2017 16:39:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/LS0-Fault-of-S12VR/m-p/656974#M13896</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2017-01-04T16:39:46Z</dc:date>
    </item>
  </channel>
</rss>