<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Need technical support in operating MC9S12XEG128CAL microcontroller at 3.3V voltage level in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Need-technical-support-in-operating-MC9S12XEG128CAL/m-p/656907#M13894</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regardless of the voltage level, in simple-chip mode the MCU bus frequency can be set up to 50 MHz and so the performance of the core and peripherals is not affected.&lt;/P&gt;&lt;P&gt;In expanded mode, however, the maximal internal bus frequency (at 3.3V) is reduced to 25 MHz, as you can see in Table A-30 in the RM.&lt;/P&gt;&lt;P&gt;Regarding ADC, you can measure in range of 0-5V if VDDA = VRH = 5V and run the MCU at 3.3V (VDDR = VDDX = 3.3V). See Table A-15. ATD Operating Characteristics.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Mar 2017 19:37:03 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2017-03-16T19:37:03Z</dc:date>
    <item>
      <title>Need technical support in operating MC9S12XEG128CAL microcontroller at 3.3V voltage level</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Need-technical-support-in-operating-MC9S12XEG128CAL/m-p/656906#M13893</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Recently we migrated from HC12 (MC912DG128C) microcontroller to HCS12 (MC9S12XEG128CAL).&lt;/P&gt;&lt;P&gt;Checked the datasheet of MC9S12XEG128CAL controller and found that, this particular controller can also operate at 3.3V voltage level.&lt;/P&gt;&lt;P&gt;Currently we are using 5V power supply. Planned to migrate to 3.3V.&lt;/P&gt;&lt;P&gt;Please let me know whether this change will affect performance ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Mar 2017 09:47:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Need-technical-support-in-operating-MC9S12XEG128CAL/m-p/656906#M13893</guid>
      <dc:creator>pavithrac</dc:creator>
      <dc:date>2017-03-16T09:47:14Z</dc:date>
    </item>
    <item>
      <title>Re: Need technical support in operating MC9S12XEG128CAL microcontroller at 3.3V voltage level</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Need-technical-support-in-operating-MC9S12XEG128CAL/m-p/656907#M13894</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regardless of the voltage level, in simple-chip mode the MCU bus frequency can be set up to 50 MHz and so the performance of the core and peripherals is not affected.&lt;/P&gt;&lt;P&gt;In expanded mode, however, the maximal internal bus frequency (at 3.3V) is reduced to 25 MHz, as you can see in Table A-30 in the RM.&lt;/P&gt;&lt;P&gt;Regarding ADC, you can measure in range of 0-5V if VDDA = VRH = 5V and run the MCU at 3.3V (VDDR = VDDX = 3.3V). See Table A-15. ATD Operating Characteristics.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Mar 2017 19:37:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Need-technical-support-in-operating-MC9S12XEG128CAL/m-p/656907#M13894</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-03-16T19:37:03Z</dc:date>
    </item>
  </channel>
</rss>