<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S12XHY128 self clock and PLL in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XHY128-self-clock-and-PLL/m-p/655241#M13870</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As S12XHY series, we have self clock mode: if CME=1 and SCME=1. But i test with customer board, found that if adding some interference, it seems that can make both Oscillator circuit and PLL circuit down. Means that when CM check there is unstable in Osc. and try to swtich to self clock mode, but found there is some problems for PLL and MCU goes down. So result in MCU broke dowm.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible? Thanks.&lt;/P&gt;&lt;P&gt;If yes. And&amp;nbsp;i guess the interference goes through VDD/SS PLL. I check the RM and found that&lt;/P&gt;&lt;P&gt;'9.2.7 &lt;EM&gt;&lt;STRONG&gt;VREGEN&lt;/STRONG&gt;&lt;/EM&gt;—Optional Regulator Enable Pin&lt;BR /&gt;This optional signal is used to shutdown VREG_3V3. In that case, VDD/VSS and VDDPLL/VSSPLL&lt;BR /&gt;must be provided externally. Shutdown mode is entered with VREGEN being low. If VREGEN is high,&lt;BR /&gt;the VREG_3V3 is either in Full Performance Mode or in Reduced Power Mode.&lt;BR /&gt;For the connectivity of VREGEN, see device specification.'&lt;/P&gt;&lt;P&gt;I want to supply VDD/SS PLL externally. Do you know how we can set VREGEN? Although i guess may be it shouldn't open to customer. I hope can get some clue from you. Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Nov 2016 09:43:33 GMT</pubDate>
    <dc:creator>BoxLi</dc:creator>
    <dc:date>2016-11-14T09:43:33Z</dc:date>
    <item>
      <title>S12XHY128 self clock and PLL</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XHY128-self-clock-and-PLL/m-p/655241#M13870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As S12XHY series, we have self clock mode: if CME=1 and SCME=1. But i test with customer board, found that if adding some interference, it seems that can make both Oscillator circuit and PLL circuit down. Means that when CM check there is unstable in Osc. and try to swtich to self clock mode, but found there is some problems for PLL and MCU goes down. So result in MCU broke dowm.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible? Thanks.&lt;/P&gt;&lt;P&gt;If yes. And&amp;nbsp;i guess the interference goes through VDD/SS PLL. I check the RM and found that&lt;/P&gt;&lt;P&gt;'9.2.7 &lt;EM&gt;&lt;STRONG&gt;VREGEN&lt;/STRONG&gt;&lt;/EM&gt;—Optional Regulator Enable Pin&lt;BR /&gt;This optional signal is used to shutdown VREG_3V3. In that case, VDD/VSS and VDDPLL/VSSPLL&lt;BR /&gt;must be provided externally. Shutdown mode is entered with VREGEN being low. If VREGEN is high,&lt;BR /&gt;the VREG_3V3 is either in Full Performance Mode or in Reduced Power Mode.&lt;BR /&gt;For the connectivity of VREGEN, see device specification.'&lt;/P&gt;&lt;P&gt;I want to supply VDD/SS PLL externally. Do you know how we can set VREGEN? Although i guess may be it shouldn't open to customer. I hope can get some clue from you. Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Nov 2016 09:43:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XHY128-self-clock-and-PLL/m-p/655241#M13870</guid>
      <dc:creator>BoxLi</dc:creator>
      <dc:date>2016-11-14T09:43:33Z</dc:date>
    </item>
    <item>
      <title>Re: S12XHY128 self clock and PLL</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XHY128-self-clock-and-PLL/m-p/655242#M13871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Box,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It would be good if you can share the schematic and layout, or just part of it which is critical for this issue.&lt;/P&gt;&lt;P&gt;Also, we would like to check the clock configuration in your SW application.&lt;/P&gt;&lt;P&gt;Then we can move on with the investigation.&lt;/P&gt;&lt;P&gt;If you cannot share this publicly, follow the instruction in below guide to open a ticket:&lt;BR /&gt;&lt;A href="https://community.nxp.com/docs/DOC-329745"&gt;How to submit a new question for NXP Support&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;iggi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Nov 2016 10:37:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XHY128-self-clock-and-PLL/m-p/655242#M13871</guid>
      <dc:creator>iggi</dc:creator>
      <dc:date>2016-11-16T10:37:57Z</dc:date>
    </item>
  </channel>
</rss>