<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: DEVKIT-S12XE schematic</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/DEVKIT-S12XE-schematic/m-p/651309#M13790</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Mr. Sestak,&lt;/P&gt;&lt;P&gt;I wish to thank you for correcting the schematic for the DEVKIT-S12XE and you were very prompt in getting back to me I must say!&amp;nbsp; I can't believe how awesome the S12 series microcontrollers are.&amp;nbsp; I had an application that used the old Motorola MC6809 CPU and needed a way to implement the entire controller board into a nice single chip solution.&amp;nbsp; I thought about implementing the 6809 into an FPGA using an open source core, but, I didn't have the time to sort out the bugs in doing that so I kept searching for something rather similar in architecture to it and I discovered S12 series components by NXP.&amp;nbsp; A programming model very similar to the 6809 only without the "U" register which turned out to be simple to implement.&amp;nbsp; I didn't have to rewrite several thousand lines of assembly either!&amp;nbsp; Using an editor I simply changed LDA's to LDAA's, etc, implemented the built in timers and such to replace the bit-banger code and delay loops and the project is nearly complete!&amp;nbsp; I can do so much with the S12XE part and with the XGATE co-processor the sky is the limit.&amp;nbsp; This is the Swiss army knife of all microcontrollers and my personal opinion is I think it is being sold short by being called an automotive microcontroller.&amp;nbsp; And what makes the whole thing even neater, your DEVKIT is connect compatible with the Arduino's shields".&amp;nbsp; Your products should get the Cool Stuff Award.&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6428i81C3276C21F19EF3/image-size/large?v=v2&amp;amp;px=999" title="20170107_053317.jpg" alt="20170107_053317.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Yours truly,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 07 Jan 2017 10:47:11 GMT</pubDate>
    <dc:creator>wb9ypa</dc:creator>
    <dc:date>2017-01-07T10:47:11Z</dc:date>
    <item>
      <title>DEVKIT-S12XE schematic</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/DEVKIT-S12XE-schematic/m-p/651306#M13787</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does anyone know where I can obtain a complete schematic for the DEVKIT-S12XE board?&amp;nbsp; I've opened the PDF file from NXP's website only to find that six of the seven sheets are missing.&amp;nbsp; Only page 5 is there.&amp;nbsp; Any help would greatly appreciated.&lt;A _jive_internal="true" href="https://community.nxp.com/tags/#/?tags=devkit-s12xe"&gt;devkit-s12xe&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Dec 2016 22:54:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/DEVKIT-S12XE-schematic/m-p/651306#M13787</guid>
      <dc:creator>wb9ypa</dc:creator>
      <dc:date>2016-12-29T22:54:24Z</dc:date>
    </item>
    <item>
      <title>Re: DEVKIT-S12XE schematic</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/DEVKIT-S12XE-schematic/m-p/651307#M13788</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;Hi Mike,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you for your bug report.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;You are right, the pdf at our web pages is wrong. I will report it to application team.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Attached is the schematic file with all pages.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jan 2017 13:12:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/DEVKIT-S12XE-schematic/m-p/651307#M13788</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2017-01-04T13:12:03Z</dc:date>
    </item>
    <item>
      <title>Re: DEVKIT-S12XE schematic</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/DEVKIT-S12XE-schematic/m-p/651308#M13789</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;UPDATE:&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.5pt; color: #262626;"&gt;Fixed. The complete schematic has been uploaded to the web page.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jan 2017 08:02:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/DEVKIT-S12XE-schematic/m-p/651308#M13789</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2017-01-05T08:02:17Z</dc:date>
    </item>
    <item>
      <title>Re: DEVKIT-S12XE schematic</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/DEVKIT-S12XE-schematic/m-p/651309#M13790</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Mr. Sestak,&lt;/P&gt;&lt;P&gt;I wish to thank you for correcting the schematic for the DEVKIT-S12XE and you were very prompt in getting back to me I must say!&amp;nbsp; I can't believe how awesome the S12 series microcontrollers are.&amp;nbsp; I had an application that used the old Motorola MC6809 CPU and needed a way to implement the entire controller board into a nice single chip solution.&amp;nbsp; I thought about implementing the 6809 into an FPGA using an open source core, but, I didn't have the time to sort out the bugs in doing that so I kept searching for something rather similar in architecture to it and I discovered S12 series components by NXP.&amp;nbsp; A programming model very similar to the 6809 only without the "U" register which turned out to be simple to implement.&amp;nbsp; I didn't have to rewrite several thousand lines of assembly either!&amp;nbsp; Using an editor I simply changed LDA's to LDAA's, etc, implemented the built in timers and such to replace the bit-banger code and delay loops and the project is nearly complete!&amp;nbsp; I can do so much with the S12XE part and with the XGATE co-processor the sky is the limit.&amp;nbsp; This is the Swiss army knife of all microcontrollers and my personal opinion is I think it is being sold short by being called an automotive microcontroller.&amp;nbsp; And what makes the whole thing even neater, your DEVKIT is connect compatible with the Arduino's shields".&amp;nbsp; Your products should get the Cool Stuff Award.&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6428i81C3276C21F19EF3/image-size/large?v=v2&amp;amp;px=999" title="20170107_053317.jpg" alt="20170107_053317.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Yours truly,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Jan 2017 10:47:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/DEVKIT-S12XE-schematic/m-p/651309#M13790</guid>
      <dc:creator>wb9ypa</dc:creator>
      <dc:date>2017-01-07T10:47:11Z</dc:date>
    </item>
  </channel>
</rss>