<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: What is the maximum current value available in S12ZVML-MINIBRD? in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/What-is-the-maximum-current-value-available-in-S12ZVML-MINIBRD/m-p/644310#M13687</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sahyun,&lt;/P&gt;&lt;P&gt;The default load current conversion slope theoretically equals 0.125 V/ 1 A when we use a 10mOhm shunt and 40k/3.2k resistor ratio for the current amplifier.&lt;/P&gt;&lt;P&gt;Since reference voltage is 2.47V and voltage ADC reference 5V, the theoretical measurable range is something below +/-20A.&lt;/P&gt;&lt;P&gt;The default I_MAX definition in source code has value 15.0.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, if you change shunt value to 1mOhm, the load current conversion slope will be 10 times smaller and the theoretical measurable range is something below +/-200A.&lt;/P&gt;&lt;P&gt;In that case, you should change the I_MAX value.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Of course, you should also change FreeMASTER Scale Variable FM_I_SCALE for correct display of current value in FreeMaster.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Aug 2017 07:22:27 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2017-08-23T07:22:27Z</dc:date>
    <item>
      <title>What is the maximum current value available in S12ZVML-MINIBRD?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/What-is-the-maximum-current-value-available-in-S12ZVML-MINIBRD/m-p/644307#M13684</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #212121; background-color: #ffffff;"&gt;I'm using S12ZVM-MINIBRD.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #212121; background-color: #ffffff;"&gt;&lt;SPAN&gt;In the datasheet, it is indicated that current can be flowed up to 20A.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #212121; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #212121; background-color: #ffffff;"&gt;&lt;SPAN style="background-color: #ffffff;"&gt;If I modify the circuit in which I sense the current, can I use a higher capacity motor?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Apr 2017 10:46:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/What-is-the-maximum-current-value-available-in-S12ZVML-MINIBRD/m-p/644307#M13684</guid>
      <dc:creator>cheolminlee</dc:creator>
      <dc:date>2017-04-03T10:46:09Z</dc:date>
    </item>
    <item>
      <title>Re: What is the maximum current value available in S12ZVML-MINIBRD?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/What-is-the-maximum-current-value-available-in-S12ZVML-MINIBRD/m-p/644308#M13685</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi CheolMin,&lt;/P&gt;&lt;P&gt;The S12ZVM-MINIBRD board was designed for +/-10A currents.&lt;/P&gt;&lt;P&gt;If you want to use higher loads, I would like to recommend:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Change shunt resistor for keep current sense signal in ADC range.&lt;/LI&gt;&lt;LI&gt;Mount silicone isolator and heatsink from the bottom side of PCB.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;That should allow you to use a higher capacity motor with S12ZVM-MINIBRD board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The heat sink should be rather bigger on (for example 5k/W) for playing on the table and lately, it may be optimized for smaller dimensions. The mounting hole at PCB should help you with proper heat sink holding.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Apr 2017 13:42:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/What-is-the-maximum-current-value-available-in-S12ZVML-MINIBRD/m-p/644308#M13685</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2017-04-03T13:42:27Z</dc:date>
    </item>
    <item>
      <title>Re: What is the maximum current value available in S12ZVML-MINIBRD?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/What-is-the-maximum-current-value-available-in-S12ZVML-MINIBRD/m-p/644309#M13686</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;&lt;STRONG&gt;Radek Sestak&lt;/STRONG&gt;&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wonder that if I change the shunt registor(to 1m ohm from 10m ohm), which parameter I modify (to reflect the modified shunt resistance)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use PMSM FOC Sensorless single shunt (AN5327) SW and MCAT tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;@ &lt;A _jive_internal="true" href="https://community.nxp.com/thread/448382?commentID=893328#comment" title="메시지로 이동"&gt;&lt;SPAN style="color: #0066cc; text-decoration: underline;"&gt;Radek Sestak&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Aug 2017 02:28:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/What-is-the-maximum-current-value-available-in-S12ZVML-MINIBRD/m-p/644309#M13686</guid>
      <dc:creator>sohyunjang</dc:creator>
      <dc:date>2017-08-23T02:28:41Z</dc:date>
    </item>
    <item>
      <title>Re: What is the maximum current value available in S12ZVML-MINIBRD?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/What-is-the-maximum-current-value-available-in-S12ZVML-MINIBRD/m-p/644310#M13687</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sahyun,&lt;/P&gt;&lt;P&gt;The default load current conversion slope theoretically equals 0.125 V/ 1 A when we use a 10mOhm shunt and 40k/3.2k resistor ratio for the current amplifier.&lt;/P&gt;&lt;P&gt;Since reference voltage is 2.47V and voltage ADC reference 5V, the theoretical measurable range is something below +/-20A.&lt;/P&gt;&lt;P&gt;The default I_MAX definition in source code has value 15.0.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, if you change shunt value to 1mOhm, the load current conversion slope will be 10 times smaller and the theoretical measurable range is something below +/-200A.&lt;/P&gt;&lt;P&gt;In that case, you should change the I_MAX value.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Of course, you should also change FreeMASTER Scale Variable FM_I_SCALE for correct display of current value in FreeMaster.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Aug 2017 07:22:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/What-is-the-maximum-current-value-available-in-S12ZVML-MINIBRD/m-p/644310#M13687</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2017-08-23T07:22:27Z</dc:date>
    </item>
  </channel>
</rss>