<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRD9Z1J638 debugging problems</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/RD9Z1J638-debugging-problems/m-p/638334#M13594</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,all&lt;/P&gt;&lt;P&gt;I download the program into the microcontroller(MM9Z1J638) by multilink universal. But &amp;nbsp;a problem accurs, The console is as follows, &amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't know what's wrong with my operation.&amp;nbsp;&lt;/P&gt;&lt;P&gt;expect to get the result soon !&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;fl::target -b 0x1000 0x2000&lt;BR /&gt;fl::target -v off -l off&lt;BR /&gt;cmdwin::fl::device -d "MM9Z1J638_FLASH" -o "128Kx32x1" -a 0xfe0000 0xffffff&lt;BR /&gt;cmdwin::fl::image -f "E:\\BMS 638 System\\RD9Z1-638-4Li-SW_Rel1.03\\MM9Z1J638\\RD9Z1-638-4Li-Sw.elf" -t "Auto Detect" -re on -r 0xfe0000 0xffffff -oe off&lt;BR /&gt;cmdwin::fl::erase image&lt;BR /&gt; Beginning Operation ... &lt;BR /&gt;------------------------- &lt;BR /&gt;Auto-detection is successful. &lt;BR /&gt; File is of type Elf Format. &lt;BR /&gt; &lt;BR /&gt;Performing target initialization ... &lt;BR /&gt;Device MM9Z1J638_FLASH is protected &lt;BR /&gt; Erasing ....&lt;BR /&gt;Error: Erase Command Failed. Operation timeout. Security area should not be programmed with a value that leads to irreversible secure &lt;BR /&gt;. Protect violation error.&lt;BR /&gt;Device MM9Z1J638_FLASH &lt;BR /&gt;An invalid preference was passed to the GDI protocol plugin(HC/RS/S12Z GDI Protocol Adapter)&lt;BR /&gt;Error: Erase Command Failed.Operation timeout. Security area should not be programmed with a value that leads to irreversible secu&lt;BR /&gt;re&lt;BR /&gt;. Protect violation error.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Nov 2016 13:47:16 GMT</pubDate>
    <dc:creator>lizhi</dc:creator>
    <dc:date>2016-11-30T13:47:16Z</dc:date>
    <item>
      <title>RD9Z1J638 debugging problems</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/RD9Z1J638-debugging-problems/m-p/638334#M13594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,all&lt;/P&gt;&lt;P&gt;I download the program into the microcontroller(MM9Z1J638) by multilink universal. But &amp;nbsp;a problem accurs, The console is as follows, &amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't know what's wrong with my operation.&amp;nbsp;&lt;/P&gt;&lt;P&gt;expect to get the result soon !&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;fl::target -b 0x1000 0x2000&lt;BR /&gt;fl::target -v off -l off&lt;BR /&gt;cmdwin::fl::device -d "MM9Z1J638_FLASH" -o "128Kx32x1" -a 0xfe0000 0xffffff&lt;BR /&gt;cmdwin::fl::image -f "E:\\BMS 638 System\\RD9Z1-638-4Li-SW_Rel1.03\\MM9Z1J638\\RD9Z1-638-4Li-Sw.elf" -t "Auto Detect" -re on -r 0xfe0000 0xffffff -oe off&lt;BR /&gt;cmdwin::fl::erase image&lt;BR /&gt; Beginning Operation ... &lt;BR /&gt;------------------------- &lt;BR /&gt;Auto-detection is successful. &lt;BR /&gt; File is of type Elf Format. &lt;BR /&gt; &lt;BR /&gt;Performing target initialization ... &lt;BR /&gt;Device MM9Z1J638_FLASH is protected &lt;BR /&gt; Erasing ....&lt;BR /&gt;Error: Erase Command Failed. Operation timeout. Security area should not be programmed with a value that leads to irreversible secure &lt;BR /&gt;. Protect violation error.&lt;BR /&gt;Device MM9Z1J638_FLASH &lt;BR /&gt;An invalid preference was passed to the GDI protocol plugin(HC/RS/S12Z GDI Protocol Adapter)&lt;BR /&gt;Error: Erase Command Failed.Operation timeout. Security area should not be programmed with a value that leads to irreversible secu&lt;BR /&gt;re&lt;BR /&gt;. Protect violation error.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Nov 2016 13:47:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/RD9Z1J638-debugging-problems/m-p/638334#M13594</guid>
      <dc:creator>lizhi</dc:creator>
      <dc:date>2016-11-30T13:47:16Z</dc:date>
    </item>
    <item>
      <title>Re: RD9Z1J638 debugging problems</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/RD9Z1J638-debugging-problems/m-p/638335#M13595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;Hi Li,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I suppose, that you use one of the small reference designs like RD9Z1-638-12V and not KIT9Z1J638EVM evaluation board. Correct?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please specify which board you use.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;According to your description, it looks like some issue with BDM connection.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please check BDM connector orientation on both sides (at the board and in BDM multilink).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The MCU must be powered from some voltage source during programming. The Multilink debugger does not provide a power supply for MCU. &amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If you use KIT9Z1J638EVM evaluation board, please check DIP switch configuration for onboard/external BDM interface.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Dec 2016 11:04:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/RD9Z1J638-debugging-problems/m-p/638335#M13595</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2016-12-01T11:04:45Z</dc:date>
    </item>
  </channel>
</rss>