<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: Sleep Mode for S12ZVL</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Sleep-Mode-for-S12ZVL/m-p/634822#M13540</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am sorry but i don;t understand what you are saying here.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In Pseudo Stop mode - In this mode the system clocks are stopped but the oscillator is still running and&lt;BR /&gt;the real time interrupt (RTI), watchdog (COP) and Autonomous Periodic Interrupt (API) may&lt;BR /&gt;be enabled. Other peripherals are turned off. This mode consumes more current than system&lt;BR /&gt;STOP mode but, as the oscillator continues to run, the full speed wake up time from this mode&lt;BR /&gt;is significantly shorter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here are some SW example demonstrating Stop mode functionality:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-330295"&gt;SW examples for MagniV S12ZVC and S12ZVL devices&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;or this one (you can re-use main.c for S12ZVL)&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-173312"&gt;Low power mode example code for MagniV S12ZVC device&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;iggi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Oct 2016 07:48:34 GMT</pubDate>
    <dc:creator>iggi</dc:creator>
    <dc:date>2016-10-17T07:48:34Z</dc:date>
    <item>
      <title>Sleep Mode for S12ZVL</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Sleep-Mode-for-S12ZVL/m-p/634821#M13539</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sleep function: When an event occurs when the time, 25 ± 0.1 seconds, the system shut down all the load, the system into the sleep mode;Sleep Mode for S12ZVL.&lt;/P&gt;&lt;P&gt;C&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;an S12ZVL achieve this function?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;Can S12 resume sleep before S12 wake up from sleep mode?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;If I choose the &lt;SPAN style="font-size: 12pt; color: #000000; font-style: normal; font-variant: normal;"&gt;&lt;STRONG&gt;Pseudo Stop Mode,is this mode？ &lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;Thanks!&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Oct 2016 01:06:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Sleep-Mode-for-S12ZVL/m-p/634821#M13539</guid>
      <dc:creator>DELPHI_Eric</dc:creator>
      <dc:date>2016-10-14T01:06:48Z</dc:date>
    </item>
    <item>
      <title>Re: Sleep Mode for S12ZVL</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Sleep-Mode-for-S12ZVL/m-p/634822#M13540</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am sorry but i don;t understand what you are saying here.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In Pseudo Stop mode - In this mode the system clocks are stopped but the oscillator is still running and&lt;BR /&gt;the real time interrupt (RTI), watchdog (COP) and Autonomous Periodic Interrupt (API) may&lt;BR /&gt;be enabled. Other peripherals are turned off. This mode consumes more current than system&lt;BR /&gt;STOP mode but, as the oscillator continues to run, the full speed wake up time from this mode&lt;BR /&gt;is significantly shorter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here are some SW example demonstrating Stop mode functionality:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-330295"&gt;SW examples for MagniV S12ZVC and S12ZVL devices&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;or this one (you can re-use main.c for S12ZVL)&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-173312"&gt;Low power mode example code for MagniV S12ZVC device&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;iggi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Oct 2016 07:48:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Sleep-Mode-for-S12ZVL/m-p/634822#M13540</guid>
      <dc:creator>iggi</dc:creator>
      <dc:date>2016-10-17T07:48:34Z</dc:date>
    </item>
  </channel>
</rss>