<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: How can I read out each device unique ID for S12G48 MCU?</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-I-read-out-each-device-unique-ID-for-S12G48-MCU/m-p/624241#M13366</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;The MCU has own lot tracking (Device ID; 8B at global address 0x0_4000 – 0x0_4007) which is supposed to be unique, since it is batch, wafer number, and x/y coordinates. However, I am not sure whether the lot number may repeat for example (it is always a 5digit number, and it numbers all the lots thru in the fab, not just for this part).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Unfortunately, the closer information about tracking number is not public.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The global memory from 0x0_4000 is accessible when we set NVMRES bit (MMCCTL1=0x01;) at PPAGE 0x01 and memory window 0x8000~0xBFFF.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The best solution is programming the own serial number into Program Once Field - 64B at global address 0x0_40C0 – 0x0_40FF. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Jan 2017 16:19:44 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2017-01-19T16:19:44Z</dc:date>
    <item>
      <title>How can I read out each device unique ID for S12G48 MCU?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-I-read-out-each-device-unique-ID-for-S12G48-MCU/m-p/624240#M13365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, guys,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could any one tell me that how can I read out each device unique ID for S12G48 MCU? Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jan 2017 13:08:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-I-read-out-each-device-unique-ID-for-S12G48-MCU/m-p/624240#M13365</guid>
      <dc:creator>csaqbz</dc:creator>
      <dc:date>2017-01-17T13:08:15Z</dc:date>
    </item>
    <item>
      <title>Re: How can I read out each device unique ID for S12G48 MCU?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-I-read-out-each-device-unique-ID-for-S12G48-MCU/m-p/624241#M13366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;The MCU has own lot tracking (Device ID; 8B at global address 0x0_4000 – 0x0_4007) which is supposed to be unique, since it is batch, wafer number, and x/y coordinates. However, I am not sure whether the lot number may repeat for example (it is always a 5digit number, and it numbers all the lots thru in the fab, not just for this part).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Unfortunately, the closer information about tracking number is not public.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The global memory from 0x0_4000 is accessible when we set NVMRES bit (MMCCTL1=0x01;) at PPAGE 0x01 and memory window 0x8000~0xBFFF.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The best solution is programming the own serial number into Program Once Field - 64B at global address 0x0_40C0 – 0x0_40FF. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jan 2017 16:19:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-I-read-out-each-device-unique-ID-for-S12G48-MCU/m-p/624241#M13366</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2017-01-19T16:19:44Z</dc:date>
    </item>
    <item>
      <title>Re: How can I read out each device unique ID for S12G48 MCU?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-I-read-out-each-device-unique-ID-for-S12G48-MCU/m-p/624242#M13367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My customer (Autoliv) has the same question for S12XE and for S12Z MagniV. &lt;/P&gt;&lt;P&gt;Is the same information (batch, wafer number, x, y coordinates) available for these devices ?&lt;/P&gt;&lt;P&gt;Thanks !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Sep 2017 13:17:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-I-read-out-each-device-unique-ID-for-S12G48-MCU/m-p/624242#M13367</guid>
      <dc:creator>yvesbriant</dc:creator>
      <dc:date>2017-09-27T13:17:35Z</dc:date>
    </item>
    <item>
      <title>Re: How can I read out each device unique ID for S12G48 MCU?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-I-read-out-each-device-unique-ID-for-S12G48-MCU/m-p/624243#M13368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yves,&lt;/P&gt;&lt;P&gt;yes, the Device ID at S12XE should work the same or very similar way as on S12G.&lt;/P&gt;&lt;P&gt;The global address in this case is &lt;SPAN&gt;0x40_0000 – 0x40_0007.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I hope it help you.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Radek&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Sep 2017 08:44:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-I-read-out-each-device-unique-ID-for-S12G48-MCU/m-p/624243#M13368</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2017-09-29T08:44:22Z</dc:date>
    </item>
  </channel>
</rss>