<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: Firmware update and FPROT</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Firmware-update-and-FPROT/m-p/609698#M13172</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;P-Flash protection [FPROT] can only be added and not removed. If you need to frequently change the protection, you can use Memory Protection Unit (MPU).&lt;/P&gt;&lt;P&gt;The Backdoor key is a security feature. Normally, the backdoor key value is not stored within the application data and should be received from an external source. But you can use it as well.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;MPU and backdoor key examples are attached.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 16 Apr 2017 18:58:53 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2017-04-16T18:58:53Z</dc:date>
    <item>
      <title>Firmware update and FPROT</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Firmware-update-and-FPROT/m-p/609697#M13171</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to be able to update the firmware on my 9sXEQ384.&lt;/P&gt;&lt;P&gt;I have the above process working but if I write to the FPROT register then I have no way to start my firmware update as I immediatly get an access violation when I start the Flash erase cycle.&amp;nbsp; The manual says this will happen also.&amp;nbsp; At the moment I leave the FPROT = 0xff and I can do a firmware update.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now can I write the backdoor key or is there any other way to do this as I would not like to leave the flash un-protected the way I have it at the moment?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an enable process that has to be done before I start a firmware update.&amp;nbsp; Ideally this process would also "modify" FPROT so that I can erase the flash .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Wade&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Apr 2017 09:13:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Firmware-update-and-FPROT/m-p/609697#M13171</guid>
      <dc:creator>dastek</dc:creator>
      <dc:date>2017-04-13T09:13:24Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware update and FPROT</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Firmware-update-and-FPROT/m-p/609698#M13172</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;P-Flash protection [FPROT] can only be added and not removed. If you need to frequently change the protection, you can use Memory Protection Unit (MPU).&lt;/P&gt;&lt;P&gt;The Backdoor key is a security feature. Normally, the backdoor key value is not stored within the application data and should be received from an external source. But you can use it as well.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;MPU and backdoor key examples are attached.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 16 Apr 2017 18:58:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Firmware-update-and-FPROT/m-p/609698#M13172</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-04-16T18:58:53Z</dc:date>
    </item>
  </channel>
</rss>