<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックS12XHY SCM</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XHY-SCM/m-p/602517#M13085</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; My customer already use S12XHY to develop the cluster project. Now they need to pass the 25KV ESD test but S12XHY is always reset. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;So i suggest customer use the clock monitor reset different reset&amp;nbsp;address to solve the cluster reset issue. &amp;nbsp;I write a test code which will force MCU reset when external OSC signal is disturbed. But what i find is very strange. When i input a disturbed noise into the external OSC input pin first time, &lt;STRONG&gt;the MCU is reset with the same power on reset address. &amp;nbsp;Then i continue to input the noise to the OSC input pin, the MCU is always into the SCM mode without any reset.&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;My quesions is:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;1. how to into the clock monitor reset address?&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;2. Why MCU can not be reset &amp;nbsp;when i input the noise into the OSC input pin after the first time?&lt;/EM&gt;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Thanks&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Best wishes&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Mike Cao&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-339245"&gt;xingtongda.7z.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Nov 2016 17:24:34 GMT</pubDate>
    <dc:creator>MikeCao</dc:creator>
    <dc:date>2016-11-17T17:24:34Z</dc:date>
    <item>
      <title>S12XHY SCM</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XHY-SCM/m-p/602517#M13085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; My customer already use S12XHY to develop the cluster project. Now they need to pass the 25KV ESD test but S12XHY is always reset. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;So i suggest customer use the clock monitor reset different reset&amp;nbsp;address to solve the cluster reset issue. &amp;nbsp;I write a test code which will force MCU reset when external OSC signal is disturbed. But what i find is very strange. When i input a disturbed noise into the external OSC input pin first time, &lt;STRONG&gt;the MCU is reset with the same power on reset address. &amp;nbsp;Then i continue to input the noise to the OSC input pin, the MCU is always into the SCM mode without any reset.&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;My quesions is:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;1. how to into the clock monitor reset address?&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;2. Why MCU can not be reset &amp;nbsp;when i input the noise into the OSC input pin after the first time?&lt;/EM&gt;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Thanks&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Best wishes&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Mike Cao&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-339245"&gt;xingtongda.7z.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Nov 2016 17:24:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XHY-SCM/m-p/602517#M13085</guid>
      <dc:creator>MikeCao</dc:creator>
      <dc:date>2016-11-17T17:24:34Z</dc:date>
    </item>
    <item>
      <title>Re: S12XHY SCM</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XHY-SCM/m-p/602518#M13086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It looks like this thread is the same as this on here&lt;A href="https://community.nxp.com/thread/438748"&gt;https://community.nxp.com/thread/438748&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But we never got a feedback...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;iggi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Nov 2016 14:57:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XHY-SCM/m-p/602518#M13086</guid>
      <dc:creator>iggi</dc:creator>
      <dc:date>2016-11-24T14:57:39Z</dc:date>
    </item>
  </channel>
</rss>