<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: S12ZVL internal Oscillator PLL</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL-internal-Oscillator-PLL/m-p/591671#M12965</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rajiv,&lt;/P&gt;&lt;P&gt;The maxim bus clock frequency for S12ZVL is 32MHz.&lt;/P&gt;&lt;P&gt;In that case, the CPMUSYNR value should be 0x5F, CPMUREFDV value should be 0x00, CPMUPOSDIV value should be 0x00.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: We know about some issues with some versions of PEmicro/OSBDM interfaces when bus clock is close to their maximum value. In that case, please go to Debug Configuration-Target settings-Edit and uncheck “Use Bus Clock as Debug Controller (SIBDC) Clock Source”. The BDM will run of 1MHz in this case.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/37896iE09BBCE99BD61A73/image-size/large?v=v2&amp;amp;px=999" title="Do not use bus clock for debug CW10.png" alt="Do not use bus clock for debug CW10.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The loading code and debugging may be slower, but more stable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may also try to download and instal the newest PEmicro/OSBDM drivers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PLL example codes:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-330238"&gt;S12ZVM clock module and PLL configuration - SW examples&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Jul 2016 09:22:42 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2016-07-20T09:22:42Z</dc:date>
    <item>
      <title>S12ZVL internal Oscillator PLL</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL-internal-Oscillator-PLL/m-p/591670#M12964</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Are there any the limitations of using internal 1MHz oscillator to get highest Bus frequency (32MHz for S12ZVL)? On my board I am not able to go above 16 MHz bus Freq.&amp;nbsp; With NXP's TRK-S12ZVL, I cannot go beyond 25MHZ. To me looks like some issue in the layout, but even with TRK-S12ZVL board (will surely be multi layer board) why not possible to achieve 32MHz Bus. Any special precautions?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Rajiv. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jul 2016 07:20:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL-internal-Oscillator-PLL/m-p/591670#M12964</guid>
      <dc:creator>rajivbandodkar</dc:creator>
      <dc:date>2016-07-20T07:20:22Z</dc:date>
    </item>
    <item>
      <title>Re: S12ZVL internal Oscillator PLL</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL-internal-Oscillator-PLL/m-p/591671#M12965</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rajiv,&lt;/P&gt;&lt;P&gt;The maxim bus clock frequency for S12ZVL is 32MHz.&lt;/P&gt;&lt;P&gt;In that case, the CPMUSYNR value should be 0x5F, CPMUREFDV value should be 0x00, CPMUPOSDIV value should be 0x00.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: We know about some issues with some versions of PEmicro/OSBDM interfaces when bus clock is close to their maximum value. In that case, please go to Debug Configuration-Target settings-Edit and uncheck “Use Bus Clock as Debug Controller (SIBDC) Clock Source”. The BDM will run of 1MHz in this case.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/37896iE09BBCE99BD61A73/image-size/large?v=v2&amp;amp;px=999" title="Do not use bus clock for debug CW10.png" alt="Do not use bus clock for debug CW10.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The loading code and debugging may be slower, but more stable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may also try to download and instal the newest PEmicro/OSBDM drivers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PLL example codes:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-330238"&gt;S12ZVM clock module and PLL configuration - SW examples&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jul 2016 09:22:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL-internal-Oscillator-PLL/m-p/591671#M12965</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2016-07-20T09:22:42Z</dc:date>
    </item>
  </channel>
</rss>