<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックMC9S12ZV32 5V Output Current Max?</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZV32-5V-Output-Current-Max/m-p/591552#M12960</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 14pt;"&gt;VDDX pin maximum current? &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 14pt;"&gt;if BCTL Control PNP Use BCP53-10(SOT223)&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Jul 2016 03:00:32 GMT</pubDate>
    <dc:creator>zongliangchan</dc:creator>
    <dc:date>2016-07-20T03:00:32Z</dc:date>
    <item>
      <title>MC9S12ZV32 5V Output Current Max?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZV32-5V-Output-Current-Max/m-p/591552#M12960</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 14pt;"&gt;VDDX pin maximum current? &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 14pt;"&gt;if BCTL Control PNP Use BCP53-10(SOT223)&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jul 2016 03:00:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZV32-5V-Output-Current-Max/m-p/591552#M12960</guid>
      <dc:creator>zongliangchan</dc:creator>
      <dc:date>2016-07-20T03:00:32Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S12ZV32 5V Output Current Max?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZV32-5V-Output-Current-Max/m-p/591553#M12961</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt; font-family: arial,helvetica,sans-serif;"&gt;Hi Zong, &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif; font-size: 12pt;"&gt;The current we can draw from the external ballast depends on the base current and gain of the&amp;nbsp; external ballast transistor.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif; font-size: 12pt;"&gt;The maximum current we can draw from external ballast transistor and supply VDDX rail is about power dissipation and thermal characteristics. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12pt; font-family: arial,helvetica,sans-serif;"&gt;The user must ensure that the maximum junction temperature is not exceeded.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12pt; font-family: arial,helvetica,sans-serif;"&gt;It depends on ambient temperature, thermal package characteristics and MCU power dissipation.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12pt; font-family: arial,helvetica,sans-serif;"&gt;MCU power has to be calculated for the particular application. This is explained in RM section A.1.6.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12pt; font-family: arial,helvetica,sans-serif;"&gt;For more details about this topic see application note below and section 3.2.2 PNP external ballast transistor:&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;A href="http://cache.nxp.com/files/microcontrollers/doc/app_note/AN5084.pdf?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1"&gt;&lt;SPAN class="l"&gt;&lt;SPAN class="goog-trans-section l"&gt;AN5084, Hardware Design Guidelines for S12ZVL Microcontrollers-Application n &lt;SPAN class="highlight"&gt;...&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/A&gt;&lt;SPAN class="toggle-preview"&gt; &lt;/SPAN&gt; (REV 1)&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;iggi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jul 2016 09:05:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZV32-5V-Output-Current-Max/m-p/591553#M12961</guid>
      <dc:creator>iggi</dc:creator>
      <dc:date>2016-07-20T09:05:44Z</dc:date>
    </item>
  </channel>
</rss>