<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: &amp;quot;Device is secure. Erase to unsecure?&amp;quot; error message comes up when I try to program MM9Z1J638 with P&amp;E's Multilink Universal. How can I reprogram MM9Z1638?</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/quot-Device-is-secure-Erase-to-unsecure-quot-error-message-comes/m-p/561108#M12802</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kadir,&lt;/P&gt;&lt;P&gt;Please check S1 switch position.&lt;/P&gt;&lt;P&gt;There are two different settings for OSBDM and external debugger.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you use OSBDM interface, please move switch 1 to the right side and switches 2, 3 and 4 to the left side.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60633iA82ABBB140E64709/image-size/large?v=v2&amp;amp;px=999" title="KIT9Z1J638EVM-BDM settings.png" alt="KIT9Z1J638EVM-BDM settings.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The D6 and D7 have to glow.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Jun 2016 13:39:02 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2016-06-27T13:39:02Z</dc:date>
    <item>
      <title>"Device is secure. Erase to unsecure?" error message comes up when I try to program MM9Z1J638 with P&amp;E's Multilink Universal. How can I reprogram MM9Z1638?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/quot-Device-is-secure-Erase-to-unsecure-quot-error-message-comes/m-p/561105#M12799</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a PCB board with MM9Z1638 on it. I was able to program it previously but something strange occured and I am no longer able to program it. Each time "it says device is secure. erase to unsecure?" When I click on yes, either this message pops up or a page with diffferent frequency options pops up. I really do not know how to fix. I looked for it on web pages, but no single solution that work is explained in details so I couldn't understand or apply existing solutions on web. &lt;/P&gt;&lt;P&gt;If I can receive your help, I will be glad. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jun 2016 11:16:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/quot-Device-is-secure-Erase-to-unsecure-quot-error-message-comes/m-p/561105#M12799</guid>
      <dc:creator>kadiruzun</dc:creator>
      <dc:date>2016-06-22T11:16:45Z</dc:date>
    </item>
    <item>
      <title>Re: "Device is secure. Erase to unsecure?" error message comes up when I try to program MM9Z1J638 with P&amp;E's Multilink Universal. How can I reprogram MM9Z1638?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/quot-Device-is-secure-Erase-to-unsecure-quot-error-message-comes/m-p/561106#M12800</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I expect the reason is not a secured device. Can you check the following items:&lt;/P&gt;&lt;P&gt;1. The device uC is not power / in sleep mode. Check if the "TRGPWR" LED is on.Otherwise wakeup the device (e.g. LIN) or power down/on.&lt;/P&gt;&lt;P&gt;2. the analog die watchdog is causing interruptions during programming:&lt;/P&gt;&lt;P&gt;During programming ONLY -&amp;nbsp; disconnect the RESET &amp;lt;&amp;gt; RESET_A line (e.g on KT9Z1_638EVM DIP S1-1 to OFF or "filter" by connecting a 470nF capacitor between RESET line and GND (pin 2 and 4 on the 6pin standard connector).&lt;/P&gt;&lt;P&gt;The best way is to solder an adapter, which can be connected on demand:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60392i5CF811FA348C2BFF/image-size/large?v=v2&amp;amp;px=999" title="adapter470nf.png" alt="adapter470nf.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;3. In general the programming tool sw (e.g. CodeWarrior 10 for MCU) should handle a secured device. There is also a &lt;SPAN class="st"&gt;UNSECURE12 tool available on the PEMicro website.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jun 2016 13:26:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/quot-Device-is-secure-Erase-to-unsecure-quot-error-message-comes/m-p/561106#M12800</guid>
      <dc:creator>Q_man</dc:creator>
      <dc:date>2016-06-23T13:26:58Z</dc:date>
    </item>
    <item>
      <title>Re: "Device is secure. Erase to unsecure?" error message comes up when I try to program MM9Z1J638 with P&amp;E's Multilink Universal. How can I reprogram MM9Z1638?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/quot-Device-is-secure-Erase-to-unsecure-quot-error-message-comes/m-p/561107#M12801</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked MCU and it is power on. At first programming I have not used 470nF cap. later on it said that device is secure. At that point I realized that I need to put a 470nF cap, and I did that. Eventhough I put that capacitor, I cannot communicate with the board. Then I checked UNSECURE12, but I think it is not compatible with MM9Z1J638. There are only HC12 type MCUs on the list.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Parallel Port 1 (and the others like 2,3,...):Not detected" status does not change even though multilink shows that I connected it to board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any other solution? Or could you please explain me how I should apply all of these in more details?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your consideration.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jun 2016 13:41:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/quot-Device-is-secure-Erase-to-unsecure-quot-error-message-comes/m-p/561107#M12801</guid>
      <dc:creator>kadiruzun</dc:creator>
      <dc:date>2016-06-23T13:41:55Z</dc:date>
    </item>
    <item>
      <title>Re: "Device is secure. Erase to unsecure?" error message comes up when I try to program MM9Z1J638 with P&amp;E's Multilink Universal. How can I reprogram MM9Z1638?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/quot-Device-is-secure-Erase-to-unsecure-quot-error-message-comes/m-p/561108#M12802</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kadir,&lt;/P&gt;&lt;P&gt;Please check S1 switch position.&lt;/P&gt;&lt;P&gt;There are two different settings for OSBDM and external debugger.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you use OSBDM interface, please move switch 1 to the right side and switches 2, 3 and 4 to the left side.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60633iA82ABBB140E64709/image-size/large?v=v2&amp;amp;px=999" title="KIT9Z1J638EVM-BDM settings.png" alt="KIT9Z1J638EVM-BDM settings.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The D6 and D7 have to glow.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jun 2016 13:39:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/quot-Device-is-secure-Erase-to-unsecure-quot-error-message-comes/m-p/561108#M12802</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2016-06-27T13:39:02Z</dc:date>
    </item>
    <item>
      <title>Re: "Device is secure. Erase to unsecure?" error message comes up when I try to program MM9Z1J638 with P&amp;E's Multilink Universal. How can I reprogram MM9Z1638?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/quot-Device-is-secure-Erase-to-unsecure-quot-error-message-comes/m-p/561109#M12803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your recommendations and solution strategies. I have figured out that this message pops up since I forgot to disable analog watchdog. It resets Digital die, which causes this problem. After I tried again and again with a piece of code which disables analog watchdog, I handled this problem. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for late reply.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2016 08:09:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/quot-Device-is-secure-Erase-to-unsecure-quot-error-message-comes/m-p/561109#M12803</guid>
      <dc:creator>kadiruzun</dc:creator>
      <dc:date>2016-07-12T08:09:24Z</dc:date>
    </item>
    <item>
      <title>Re: "Device is secure. Erase to unsecure?" error message comes up when I try to program MM9Z1J638 with P&amp;E's Multilink Universal. How can I reprogram MM9Z1638?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/quot-Device-is-secure-Erase-to-unsecure-quot-error-message-comes/m-p/561110#M12804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kadir,&lt;/P&gt;&lt;P&gt;You're welcome.&lt;/P&gt;&lt;P&gt;I am glad that the problem has been resolved.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2016 08:15:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/quot-Device-is-secure-Erase-to-unsecure-quot-error-message-comes/m-p/561110#M12804</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2016-07-12T08:15:23Z</dc:date>
    </item>
    <item>
      <title>Re: "Device is secure. Erase to unsecure?" error message comes up when I try to program MM9Z1J638 with P&amp;E's Multilink Universal. How can I reprogram MM9Z1638?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/quot-Device-is-secure-Erase-to-unsecure-quot-error-message-comes/m-p/561111#M12805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kadir,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;I have the same problem with yours, and I want to know how can you try again and again with a piece of code, because I can't connect to the board and download the code.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Dec 2017 05:36:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/quot-Device-is-secure-Erase-to-unsecure-quot-error-message-comes/m-p/561111#M12805</guid>
      <dc:creator>tuozhou</dc:creator>
      <dc:date>2017-12-04T05:36:00Z</dc:date>
    </item>
  </channel>
</rss>