<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC9S12 gpio injection current in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12-gpio-injection-current/m-p/547343#M12688</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Angelo,&lt;/P&gt;&lt;P&gt;In fact, every S12 MCU GPIO pin is protected by ESD diodes against power supply rails.&lt;/P&gt;&lt;P&gt;So, any voltage higher than VDDX + voltage drop at ESD diode will generate injection current.&lt;/P&gt;&lt;P&gt;The same is valid for voltage smaller than VSSX - voltage drop at ESD diode.&lt;/P&gt;&lt;P&gt;Note: VDDA/VSSA for port AD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The voltage drop at ESD diode for a fully opened diode is approximately 0.6 - 0.7V. However, we have to calculate rather with 0.3V where ESD diode starts open.&lt;/P&gt;&lt;P&gt;The maximum allowed continues injection current for one pin is 2.5mA.&lt;/P&gt;&lt;P&gt;However, the ESD diodes are not designed continuous conducting current and therefore we should avoid that situation if possible. It might have also side effects:&lt;/P&gt;&lt;P&gt;The ESD diode is heated by this injected current and influence neighborhood silicon.&lt;/P&gt;&lt;P&gt;The ADC results at neighborhood channels might be influenced.&lt;/P&gt;&lt;P&gt;The injection current might cause the fault (overvoltage) of the voltage regulator in MCU power save modes.&lt;/P&gt;&lt;P&gt;…&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please look at our application note AN4731 Understanding Injection Current on Freescale Automotive Microcontrollers for more details about injection current:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/files/32bit/doc/app_note/AN4731.pdf"&gt;http://www.nxp.com/files/32bit/doc/app_note/AN4731.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;You might look also on slightly older application note AN2434 Input-Output Pin Drivers on HCS12 Family MCUs:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/files/microcontrollers/doc/app_note/AN2434.pdf"&gt;http://www.nxp.com/files/microcontrollers/doc/app_note/AN2434.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and AN2433 5V to 3V Design Considerations:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/files/microcontrollers/doc/app_note/AN2433.pdf"&gt;http://www.nxp.com/files/microcontrollers/doc/app_note/AN2433.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Note: AN2433 is from 2002. There is plenty of newer voltage level translators which might be used:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/products/discretes-and-logic/logic/voltage-level-translators"&gt;http://www.nxp.com/products/discretes-and-logic/logic/voltage-level-translators&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/products/interface-and-connectivity/interface-and-system-management/ic-bus-portfolio/ic-voltage-level-translators"&gt;http://www.nxp.com/products/interface-and-connectivity/interface-and-system-management/ic-bus-portfolio/ic-voltage-level-translators&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Jul 2016 12:05:22 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2016-07-28T12:05:22Z</dc:date>
    <item>
      <title>MC9S12 gpio injection current</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12-gpio-injection-current/m-p/547342#M12687</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;trying to figure out what is the injection current if i connect a 5V level to a 3.3VI/O powered mcu.&lt;/P&gt;&lt;P&gt;From datasheet seems it can reach &amp;gt; 3mA so over suggested limits, but not sure, since the diagram&lt;/P&gt;&lt;P&gt;is showing an example case for voltages &amp;gt; 5V.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help is appreciated.&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;angelo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2016 08:02:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12-gpio-injection-current/m-p/547342#M12687</guid>
      <dc:creator>angelo_d</dc:creator>
      <dc:date>2016-07-28T08:02:02Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S12 gpio injection current</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12-gpio-injection-current/m-p/547343#M12688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Angelo,&lt;/P&gt;&lt;P&gt;In fact, every S12 MCU GPIO pin is protected by ESD diodes against power supply rails.&lt;/P&gt;&lt;P&gt;So, any voltage higher than VDDX + voltage drop at ESD diode will generate injection current.&lt;/P&gt;&lt;P&gt;The same is valid for voltage smaller than VSSX - voltage drop at ESD diode.&lt;/P&gt;&lt;P&gt;Note: VDDA/VSSA for port AD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The voltage drop at ESD diode for a fully opened diode is approximately 0.6 - 0.7V. However, we have to calculate rather with 0.3V where ESD diode starts open.&lt;/P&gt;&lt;P&gt;The maximum allowed continues injection current for one pin is 2.5mA.&lt;/P&gt;&lt;P&gt;However, the ESD diodes are not designed continuous conducting current and therefore we should avoid that situation if possible. It might have also side effects:&lt;/P&gt;&lt;P&gt;The ESD diode is heated by this injected current and influence neighborhood silicon.&lt;/P&gt;&lt;P&gt;The ADC results at neighborhood channels might be influenced.&lt;/P&gt;&lt;P&gt;The injection current might cause the fault (overvoltage) of the voltage regulator in MCU power save modes.&lt;/P&gt;&lt;P&gt;…&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please look at our application note AN4731 Understanding Injection Current on Freescale Automotive Microcontrollers for more details about injection current:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/files/32bit/doc/app_note/AN4731.pdf"&gt;http://www.nxp.com/files/32bit/doc/app_note/AN4731.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;You might look also on slightly older application note AN2434 Input-Output Pin Drivers on HCS12 Family MCUs:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/files/microcontrollers/doc/app_note/AN2434.pdf"&gt;http://www.nxp.com/files/microcontrollers/doc/app_note/AN2434.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and AN2433 5V to 3V Design Considerations:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/files/microcontrollers/doc/app_note/AN2433.pdf"&gt;http://www.nxp.com/files/microcontrollers/doc/app_note/AN2433.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Note: AN2433 is from 2002. There is plenty of newer voltage level translators which might be used:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/products/discretes-and-logic/logic/voltage-level-translators"&gt;http://www.nxp.com/products/discretes-and-logic/logic/voltage-level-translators&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/products/interface-and-connectivity/interface-and-system-management/ic-bus-portfolio/ic-voltage-level-translators"&gt;http://www.nxp.com/products/interface-and-connectivity/interface-and-system-management/ic-bus-portfolio/ic-voltage-level-translators&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2016 12:05:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12-gpio-injection-current/m-p/547343#M12688</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2016-07-28T12:05:22Z</dc:date>
    </item>
  </channel>
</rss>