<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: S912ZVCA192 Sleep, Wake Issue</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S912ZVCA192-Sleep-Wake-Issue/m-p/535937#M12595</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Firstly what you can do is to disable interrupts prior to Stop Mode just to see if that works well.&lt;/P&gt;&lt;P&gt;It is good to scan the ECLK signal on pin PT7 which is the frequency of the bus clock so you can see if the MCU runs or not.&lt;/P&gt;&lt;P&gt;Just add the following codeline:&lt;/P&gt;&lt;P&gt;ECLKCTL = 0x00; //enable free-running clock on the ECLK pin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the KWU interrupt routine your purpose of writing to CPMUARMCOP register is to trigger reset, right?&lt;/P&gt;&lt;P&gt;Note that write of 0x55 value following a write of 0xAA value in the CPMUARMCOP resets the time-out period. But still if this writes are not in loop (like in RESET_WATCHDOG function), the COP will cause a reset after time-out.&lt;/P&gt;&lt;P&gt;In this simple case flag clearing is okay, but recommendation is to do it like this:&lt;BR /&gt;PIFADL = 0x08;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Btw, ensure the switch or push button you use as key wakeup changes the logic level from 0 to 1, so you get rising edge.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also you can test this&lt;A href="https://community.nxp.com/docs/DOC-173312"&gt;Low power mode example code for MagniV S12ZVC device&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;iggi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 08:21:38 GMT</pubDate>
    <dc:creator>iggi</dc:creator>
    <dc:date>2016-06-16T08:21:38Z</dc:date>
    <item>
      <title>S912ZVCA192 Sleep, Wake Issue</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S912ZVCA192-Sleep-Wake-Issue/m-p/535936#M12594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am Using S912ZVCA192 controller. I want the controller to go to sleep mode and then wake it up with Key Wake up Interrupt.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note:1&lt;/P&gt;&lt;P&gt;I am Using&lt;/P&gt;&lt;P&gt;asm ANDCC #0x7F;&amp;nbsp; //clear S bit - enable the stop mode. If the S bit is not&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //cleared then STOP instruction has no effect and is&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //executed as a dummy instruction NOP.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm STOP;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //STOP mode&lt;/P&gt;&lt;P&gt;to go to sleep mode.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note:2&lt;/P&gt;&lt;P&gt;I am configuring KWP interrupt before executing the above Instruction.&lt;/P&gt;&lt;P&gt;/*configure port AD for KWU feature*/&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DDRAD_DDRADL3 = 0;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Configure PAD3 as input */&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; DIENADL_DIENADL3 = 1;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Pin is configured as digital input */&lt;/P&gt;&lt;P&gt;&amp;nbsp; PERAD_PERADL3 = 0;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Enable Pull Device on PAD3 */&lt;/P&gt;&lt;P&gt;&amp;nbsp; PPSAD_PPSADL3 = 1;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Configure interrupt for Rising Edge */&lt;/P&gt;&lt;P&gt;&amp;nbsp; PIEAD_PIEADL3 = 1;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Enable Interrupt on PAD3 (KWAD3) */&lt;/P&gt;&lt;P&gt;And In ISR of KWP&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;interrupt VectorNumber_Vportad HLUWAKE_INT(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PIFADL_PIFADL3=1;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CPMUCOP = 0x01;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CPMUARMCOP = 0x50U;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CPMUARMCOP = 0xA0U;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The problem is controller does not enters full stop mode.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Kiran Bhat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 07:25:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S912ZVCA192-Sleep-Wake-Issue/m-p/535936#M12594</guid>
      <dc:creator>kiranbhat</dc:creator>
      <dc:date>2016-06-16T07:25:11Z</dc:date>
    </item>
    <item>
      <title>Re: S912ZVCA192 Sleep, Wake Issue</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S912ZVCA192-Sleep-Wake-Issue/m-p/535937#M12595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Firstly what you can do is to disable interrupts prior to Stop Mode just to see if that works well.&lt;/P&gt;&lt;P&gt;It is good to scan the ECLK signal on pin PT7 which is the frequency of the bus clock so you can see if the MCU runs or not.&lt;/P&gt;&lt;P&gt;Just add the following codeline:&lt;/P&gt;&lt;P&gt;ECLKCTL = 0x00; //enable free-running clock on the ECLK pin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the KWU interrupt routine your purpose of writing to CPMUARMCOP register is to trigger reset, right?&lt;/P&gt;&lt;P&gt;Note that write of 0x55 value following a write of 0xAA value in the CPMUARMCOP resets the time-out period. But still if this writes are not in loop (like in RESET_WATCHDOG function), the COP will cause a reset after time-out.&lt;/P&gt;&lt;P&gt;In this simple case flag clearing is okay, but recommendation is to do it like this:&lt;BR /&gt;PIFADL = 0x08;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Btw, ensure the switch or push button you use as key wakeup changes the logic level from 0 to 1, so you get rising edge.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also you can test this&lt;A href="https://community.nxp.com/docs/DOC-173312"&gt;Low power mode example code for MagniV S12ZVC device&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;iggi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 08:21:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S912ZVCA192-Sleep-Wake-Issue/m-p/535937#M12595</guid>
      <dc:creator>iggi</dc:creator>
      <dc:date>2016-06-16T08:21:38Z</dc:date>
    </item>
    <item>
      <title>Re: S912ZVCA192 Sleep, Wake Issue</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S912ZVCA192-Sleep-Wake-Issue/m-p/535938#M12596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Iggi&lt;/P&gt;&lt;P&gt;Thanks for the support Issue resolved&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Kiran bhat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jun 2016 05:59:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S912ZVCA192-Sleep-Wake-Issue/m-p/535938#M12596</guid>
      <dc:creator>kiranbhat</dc:creator>
      <dc:date>2016-06-17T05:59:21Z</dc:date>
    </item>
    <item>
      <title>Re: S912ZVCA192 Sleep, Wake Issue</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S912ZVCA192-Sleep-Wake-Issue/m-p/535939#M12597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi，iggi&lt;/P&gt;&lt;P&gt;I don't know whether I can use this code in S12ZVL.I have only recently been in toch with this MCU.&lt;/P&gt;&lt;P&gt;And I want the controller just run in stop mode then waked up with Key Wake up Interrupt, as like Kiran bhat.&lt;/P&gt;&lt;P&gt;I saw the datasheet of MC9S12ZVL32.If I want it enter full stop mode,I think what i need to do is to set the bit PSTP or OSCE.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/59946iFE95866CDF72D1FD/image-size/large?v=v2&amp;amp;px=999" title="STOP_MODE-EN.jpg" alt="STOP_MODE-EN.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So I write code like this:&lt;/P&gt;&lt;P&gt;//&amp;nbsp; CPMUCLKS_PSTP=1;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; CPMUOSC_OSCE=1;&lt;/P&gt;&lt;P&gt;but it does't use.And when I debug in Code Warrior 10.6,the bit does't set.&lt;/P&gt;&lt;P&gt;By the way,my board doesn't have the external OSC,does it matter?Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;kexiangLi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 25 Jun 2016 14:01:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S912ZVCA192-Sleep-Wake-Issue/m-p/535939#M12597</guid>
      <dc:creator>kexiangli</dc:creator>
      <dc:date>2016-06-25T14:01:37Z</dc:date>
    </item>
  </channel>
</rss>