<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I am having an issue with using a fresh S12G48 microcontroller, pin 26 (PS1/TX0) appears to be shorted to ground internally, when powering the microcontroller via VDDXRA and VSSXA pins (3.3V) there is a 1.5A current draw and the MCU becomes hot. I am  in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-am-having-an-issue-with-using-a-fresh-S12G48-microcontroller/m-p/510176#M12437</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, such behavior is very unusual and that should not happen.&lt;/P&gt;&lt;P&gt;Where did you buy the parts? I hope you did it through authorized distributor network.&lt;/P&gt;&lt;P&gt;Is your HW schematic and layout board correct? Please check the schematic of our TWR-S12G64 tower board and compare it with your design if there is anything wrong.&lt;/P&gt;&lt;P&gt;It would be good if you can have the tower board and replace the micro with one from the batch to check if the MCUs are really bad.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;iggi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Mar 2016 09:19:07 GMT</pubDate>
    <dc:creator>iggi</dc:creator>
    <dc:date>2016-03-30T09:19:07Z</dc:date>
    <item>
      <title>I am having an issue with using a fresh S12G48 microcontroller, pin 26 (PS1/TX0) appears to be shorted to ground internally, when powering the microcontroller via VDDXRA and VSSXA pins (3.3V) there is a 1.5A current draw and the MCU becomes hot. I am unab</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-am-having-an-issue-with-using-a-fresh-S12G48-microcontroller/m-p/510175#M12436</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am having an issue with a fresh S12G48 MCU, pin 26 (PS1/TX0) appears to be shorted to ground internally, when powering the microcontroller via VDDXRA and VSSXA pins (3.3V) there is a 1.5A current draw and the MCU becomes hot. I am unable to program the MCU as it is not responding to the BDM programming module. I have tried multiple MCUs from the same batch and they all seem to behave in the same way. Many thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Mar 2016 13:04:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-am-having-an-issue-with-using-a-fresh-S12G48-microcontroller/m-p/510175#M12436</guid>
      <dc:creator>mihailsjakovlev</dc:creator>
      <dc:date>2016-03-29T13:04:47Z</dc:date>
    </item>
    <item>
      <title>Re: I am having an issue with using a fresh S12G48 microcontroller, pin 26 (PS1/TX0) appears to be shorted to ground internally, when powering the microcontroller via VDDXRA and VSSXA pins (3.3V) there is a 1.5A current draw and the MCU becomes hot. I am</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-am-having-an-issue-with-using-a-fresh-S12G48-microcontroller/m-p/510176#M12437</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, such behavior is very unusual and that should not happen.&lt;/P&gt;&lt;P&gt;Where did you buy the parts? I hope you did it through authorized distributor network.&lt;/P&gt;&lt;P&gt;Is your HW schematic and layout board correct? Please check the schematic of our TWR-S12G64 tower board and compare it with your design if there is anything wrong.&lt;/P&gt;&lt;P&gt;It would be good if you can have the tower board and replace the micro with one from the batch to check if the MCUs are really bad.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;iggi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Mar 2016 09:19:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-am-having-an-issue-with-using-a-fresh-S12G48-microcontroller/m-p/510176#M12437</guid>
      <dc:creator>iggi</dc:creator>
      <dc:date>2016-03-30T09:19:07Z</dc:date>
    </item>
  </channel>
</rss>