<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックMagniV S12ZVC Operate at 15V?</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MagniV-S12ZVC-Operate-at-15V/m-p/509994#M12428</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can the VLG-MC9S12ZVC evaluation board operate from a 15V power supply?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I believe that the MCU can run from 15V (is that true?), but is there anything on the evaluation board that would prevent this?&amp;nbsp; Or are there any other cautions to consider if operating from 15V?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Derrick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Jan 2016 14:18:07 GMT</pubDate>
    <dc:creator>Derrick</dc:creator>
    <dc:date>2016-01-22T14:18:07Z</dc:date>
    <item>
      <title>MagniV S12ZVC Operate at 15V?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MagniV-S12ZVC-Operate-at-15V/m-p/509994#M12428</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can the VLG-MC9S12ZVC evaluation board operate from a 15V power supply?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I believe that the MCU can run from 15V (is that true?), but is there anything on the evaluation board that would prevent this?&amp;nbsp; Or are there any other cautions to consider if operating from 15V?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Derrick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jan 2016 14:18:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MagniV-S12ZVC-Operate-at-15V/m-p/509994#M12428</guid>
      <dc:creator>Derrick</dc:creator>
      <dc:date>2016-01-22T14:18:07Z</dc:date>
    </item>
    <item>
      <title>Re: MagniV S12ZVC Operate at 15V?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MagniV-S12ZVC-Operate-at-15V/m-p/509995#M12429</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello?&amp;nbsp; Is anyone looking into this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jan 2016 14:14:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MagniV-S12ZVC-Operate-at-15V/m-p/509995#M12429</guid>
      <dc:creator>Derrick</dc:creator>
      <dc:date>2016-01-28T14:14:17Z</dc:date>
    </item>
    <item>
      <title>Re: MagniV S12ZVC Operate at 15V?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MagniV-S12ZVC-Operate-at-15V/m-p/509996#M12430</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Derrick,&lt;/P&gt;&lt;P&gt;sorry for delay.&lt;/P&gt;&lt;P&gt;I checked schematic and I do not see any problem with 15V.&lt;/P&gt;&lt;P&gt;The lowest limit is given by MCU (the standard operational range up to 18V, but it will survive 40V for short time) and Buzzer (operational range up to 20V). All other limits are above…&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jan 2016 16:45:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MagniV-S12ZVC-Operate-at-15V/m-p/509996#M12430</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2016-01-28T16:45:32Z</dc:date>
    </item>
  </channel>
</rss>