<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックS12G128 IO output current issue.</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12G128-IO-output-current-issue/m-p/507398#M12389</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;customer Gaei design 2 IO pins output continue current&amp;nbsp; equal to 10mA/ each pin. is it resenable ? the 2 pin used to diver NPN for relay.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Mar 2016 03:36:14 GMT</pubDate>
    <dc:creator>jacky_Tan</dc:creator>
    <dc:date>2016-03-04T03:36:14Z</dc:date>
    <item>
      <title>S12G128 IO output current issue.</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12G128-IO-output-current-issue/m-p/507398#M12389</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;customer Gaei design 2 IO pins output continue current&amp;nbsp; equal to 10mA/ each pin. is it resenable ? the 2 pin used to diver NPN for relay.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Mar 2016 03:36:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12G128-IO-output-current-issue/m-p/507398#M12389</guid>
      <dc:creator>jacky_Tan</dc:creator>
      <dc:date>2016-03-04T03:36:14Z</dc:date>
    </item>
    <item>
      <title>Re: S12G128 IO output current issue.</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12G128-IO-output-current-issue/m-p/507399#M12390</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Zaiqiu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It depends ….&lt;/P&gt;&lt;P&gt;1. on the power supply. S12G RM specifies minimal VOH as (4.2V) for current -4mA and 5V power supply (see Table A-8 and Table A-9).&amp;nbsp; S12G RM specifies minimal VOH as (2.9V) for current -4mA and 3.3V power supply (see Table A-6 and Table A-7). These values are worst cases with some safety gap, but it still mean that values of the output voltage may be strongly influenced by this current. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. on total consumption and selected MCU package. The maximum current for single power supply pin is +/-60mA (See Table A-1). So, if we have MCU with just one VDD pin (like VDDXRA), the total consumption of MCU include loads should be below these 60mA. The same is valid for VSS (VSSXA) pins.&lt;/P&gt;&lt;P&gt;Note: CPU is powered by VDDR domain, ports except AD are powered by VDDX domain, port AD and analog modules are powered by VDDA domain.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. circuit protection. Relays are inductive loads which may generate spikes…&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Shouldn’t be better use some MOSFETs or directly switches?&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/products/automotive-products/discrete-and-logic/automotive-mosfets:MC_50933" title="http://www.nxp.com/products/automotive-products/discrete-and-logic/automotive-mosfets:MC_50933"&gt;Automotive MOSFETs|NXP&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/products/discretes-and-logic/mosfets:MC_71128" title="http://www.nxp.com/products/discretes-and-logic/mosfets:MC_71128"&gt;MOSFETs|NXP&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another option is using S12VR MCU with integrated two low side drivers to drive inductive loads and powered directly from 12V (for higher inductive loads is here MM912_634).&lt;/P&gt;&lt;P&gt;Note: The rest of MCU is very similar to S12G family.&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/16-bit-s12-magniv/s12vr-mixed-signal-mcu-for-automotive-industrial-relay-based-motor-control:S12VR" title="http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/16-bit-s12-magniv/s12vr-mixed-signal-mcu-for-automotive-industrial-relay-based-motor-control:S12VR"&gt;S12VR Mixed-Signal MCU|MagniV|NXP&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/products/power-management/engine-and-dc-motor-control/powertrain-engine-control/integrated-hcs12-based-relay-driver-microcontrollers-mcus-with-lin:MM912_634" title="http://www.nxp.com/products/power-management/engine-and-dc-motor-control/powertrain-engine-control/integrated-hcs12-based-relay-driver-microcontrollers-mcus-with-lin:MM912_634"&gt;HCS12 Based Relay Driver with LIN|NXP&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Mar 2016 17:30:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12G128-IO-output-current-issue/m-p/507399#M12390</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2016-03-04T17:30:46Z</dc:date>
    </item>
  </channel>
</rss>