<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Parammeters setting about S12ZVM128EVB in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Parammeters-setting-about-S12ZVM128EVB/m-p/502987#M12316</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi zoujiahao,&lt;/P&gt;&lt;P&gt;Could you please specify parameters of your BLDC motor?&lt;/P&gt;&lt;P&gt;In fact, the MC9S12ZVML128_BLDC_Sensorless code has all settings directly inside MC9S12ZVML128_BLDC_Sensorless.c file.&lt;/P&gt;&lt;P&gt;The S12ZVML128EVB board contains the SW3 switch (ON/OFF) which drive motor control code. Is this switch in the correct position?&lt;/P&gt;&lt;P&gt;Please check also default jumper positions on your board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It would be great if you could look at that in FreeMaster and check why it did not run.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The motor may not rotate due to DC bus current limit. The maximum current could be modified by DC_BUS_CURRENT_LIMIT and ALIGN_CURRENT_SCALED parameters (both should contain the same value).&lt;/P&gt;&lt;P&gt;You may also try modifying ADVANCE_ANGLE parameter for tuning Back-EMF detection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 May 2016 13:06:57 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2016-05-10T13:06:57Z</dc:date>
    <item>
      <title>Parammeters setting about S12ZVM128EVB</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Parammeters-setting-about-S12ZVM128EVB/m-p/502986#M12315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello! I bought a S12ZVML128EVB, and the BLDC is not from Freescale. I had download the software MC9S12ZVML128_BLDC_Sensorless, but it can't rotate the motor. Where to set the parameters? I can't find the motor parammeters in software.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 May 2016 23:49:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Parammeters-setting-about-S12ZVM128EVB/m-p/502986#M12315</guid>
      <dc:creator>zoujiahao</dc:creator>
      <dc:date>2016-05-05T23:49:18Z</dc:date>
    </item>
    <item>
      <title>Re: Parammeters setting about S12ZVM128EVB</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Parammeters-setting-about-S12ZVM128EVB/m-p/502987#M12316</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi zoujiahao,&lt;/P&gt;&lt;P&gt;Could you please specify parameters of your BLDC motor?&lt;/P&gt;&lt;P&gt;In fact, the MC9S12ZVML128_BLDC_Sensorless code has all settings directly inside MC9S12ZVML128_BLDC_Sensorless.c file.&lt;/P&gt;&lt;P&gt;The S12ZVML128EVB board contains the SW3 switch (ON/OFF) which drive motor control code. Is this switch in the correct position?&lt;/P&gt;&lt;P&gt;Please check also default jumper positions on your board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It would be great if you could look at that in FreeMaster and check why it did not run.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The motor may not rotate due to DC bus current limit. The maximum current could be modified by DC_BUS_CURRENT_LIMIT and ALIGN_CURRENT_SCALED parameters (both should contain the same value).&lt;/P&gt;&lt;P&gt;You may also try modifying ADVANCE_ANGLE parameter for tuning Back-EMF detection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 May 2016 13:06:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Parammeters-setting-about-S12ZVM128EVB/m-p/502987#M12316</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2016-05-10T13:06:57Z</dc:date>
    </item>
    <item>
      <title>Re: Parammeters setting about S12ZVM128EVB</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Parammeters-setting-about-S12ZVM128EVB/m-p/502988#M12317</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Radek,&lt;/P&gt;&lt;P&gt;I did it by modifying &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;ADVANCE_ANGLE. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 May 2016 13:35:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Parammeters-setting-about-S12ZVM128EVB/m-p/502988#M12317</guid>
      <dc:creator>zoujiahao</dc:creator>
      <dc:date>2016-05-10T13:35:11Z</dc:date>
    </item>
  </channel>
</rss>