<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 MC9S12ZVML64MKH Code Warrior Processor Expert Generate Project</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZVML64MKH-Code-Warrior-Processor-Expert-Generate-Project/m-p/502009#M12309</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I used Code Warrior Processor Expert Generated a MC9S12ZVML64MKH&amp;nbsp; project to test the Phase voltage of BLDC, I configure all the function as attached file, but I got a static value while the phase voltage changed. Can anybody help me find the reason?&lt;/P&gt;&lt;P&gt;Thanks...&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338813"&gt;test.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Jan 2016 13:55:57 GMT</pubDate>
    <dc:creator>dannydeng</dc:creator>
    <dc:date>2016-01-19T13:55:57Z</dc:date>
    <item>
      <title>MC9S12ZVML64MKH Code Warrior Processor Expert Generate Project</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZVML64MKH-Code-Warrior-Processor-Expert-Generate-Project/m-p/502009#M12309</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I used Code Warrior Processor Expert Generated a MC9S12ZVML64MKH&amp;nbsp; project to test the Phase voltage of BLDC, I configure all the function as attached file, but I got a static value while the phase voltage changed. Can anybody help me find the reason?&lt;/P&gt;&lt;P&gt;Thanks...&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338813"&gt;test.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jan 2016 13:55:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZVML64MKH-Code-Warrior-Processor-Expert-Generate-Project/m-p/502009#M12309</guid>
      <dc:creator>dannydeng</dc:creator>
      <dc:date>2016-01-19T13:55:57Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S12ZVML64MKH Code Warrior Processor Expert Generate Project</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZVML64MKH-Code-Warrior-Processor-Expert-Generate-Project/m-p/502010#M12310</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ray,&lt;/P&gt;&lt;P&gt;I shortly checked your code and unfortunately I do not see any obvious issue there.&lt;/P&gt;&lt;P&gt;The code should measure voltage at HS1 pin (pin49) divided by 6.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I didn’t test it till now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which voltage did you connect to HS1 pin?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jan 2016 16:56:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZVML64MKH-Code-Warrior-Processor-Expert-Generate-Project/m-p/502010#M12310</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2016-01-20T16:56:18Z</dc:date>
    </item>
  </channel>
</rss>