<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic What is the difference between S12X and S12Z core ? in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/What-is-the-difference-between-S12X-and-S12Z-core/m-p/486095#M12075</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I wanted to know the difference between the S12X and S12Z core. If the things are implemented in the MCS12XDP512 can directly compatible with MC9S12ZVM.&lt;/P&gt;&lt;P&gt;Is there things that to be needs to be taken care before porting. Iam going through the stuffs available on this but I need immediate inputs on this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Jan 2016 08:15:39 GMT</pubDate>
    <dc:creator>ameykhatavkar</dc:creator>
    <dc:date>2016-01-13T08:15:39Z</dc:date>
    <item>
      <title>What is the difference between S12X and S12Z core ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/What-is-the-difference-between-S12X-and-S12Z-core/m-p/486095#M12075</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I wanted to know the difference between the S12X and S12Z core. If the things are implemented in the MCS12XDP512 can directly compatible with MC9S12ZVM.&lt;/P&gt;&lt;P&gt;Is there things that to be needs to be taken care before porting. Iam going through the stuffs available on this but I need immediate inputs on this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jan 2016 08:15:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/What-is-the-difference-between-S12X-and-S12Z-core/m-p/486095#M12075</guid>
      <dc:creator>ameykhatavkar</dc:creator>
      <dc:date>2016-01-13T08:15:39Z</dc:date>
    </item>
    <item>
      <title>Re: What is the difference between S12X and S12Z core ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/What-is-the-difference-between-S12X-and-S12Z-core/m-p/486096#M12076</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Amey,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please look at my answer here:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/604458#604458"&gt;https://community.freescale.com/message/604458#604458&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I would like to add two more specific points:&lt;/P&gt;&lt;P&gt;1. S12Z MCUs have implemented ECC on RAM and Flash (you cannot use cumulative write into Flash).&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;2. Double bit ECC error, illegal opcode and illegal address access will cause Machine exception interrupt.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jan 2016 14:30:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/What-is-the-difference-between-S12X-and-S12Z-core/m-p/486096#M12076</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2016-01-13T14:30:17Z</dc:date>
    </item>
  </channel>
</rss>