<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: problem dealing with two CANs in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-dealing-with-two-CANs/m-p/485615#M12072</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi carl,&lt;/P&gt;&lt;P&gt;Could you please specify your MCU derivative? CAN interrupts are managed by CPU or XGATE?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which version of CW you use?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Contains your CAN routines any loops which could be potentially infinite?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you implement CAN Error Interrupt routines?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suppose that CANs have independent external transceivers. Could you please check whether new data correctly arrived to MCU pins?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you sure that CAN codes do not share any global variable for processing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Jan 2016 16:54:58 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2016-01-13T16:54:58Z</dc:date>
    <item>
      <title>problem dealing with two CANs</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-dealing-with-two-CANs/m-p/485614#M12071</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am using MC9S12 MCU for a project which requires receiving messages from two separate CANs from a vehicle. The problem I am having is that one of the CAN interrupt will randomly stop receiving message from the CAN bus. when this happens, I have to restart the program again.&lt;/P&gt;&lt;P&gt;I never have this problem when dealing with receiving from one CAN. I have tried setting one CAN with high priority and another with lower priority but the problem persists. logically, I assume this happens when interrupt from one CAN happens before another CAN has finished processing the message. Is there a way to solve this problem? thanks, &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jan 2016 15:09:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-dealing-with-two-CANs/m-p/485614#M12071</guid>
      <dc:creator>karlsl</dc:creator>
      <dc:date>2016-01-12T15:09:30Z</dc:date>
    </item>
    <item>
      <title>Re: problem dealing with two CANs</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-dealing-with-two-CANs/m-p/485615#M12072</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi carl,&lt;/P&gt;&lt;P&gt;Could you please specify your MCU derivative? CAN interrupts are managed by CPU or XGATE?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which version of CW you use?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Contains your CAN routines any loops which could be potentially infinite?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you implement CAN Error Interrupt routines?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suppose that CANs have independent external transceivers. Could you please check whether new data correctly arrived to MCU pins?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you sure that CAN codes do not share any global variable for processing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jan 2016 16:54:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-dealing-with-two-CANs/m-p/485615#M12072</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2016-01-13T16:54:58Z</dc:date>
    </item>
  </channel>
</rss>