<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: MC9S12ZVCA192</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZVCA192/m-p/484286#M12053</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sumathi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to apologize, but I am not sure with your question.&lt;/P&gt;&lt;P&gt;S12ZVC contains MSCAN module and CANPHY (CAN transceiver).&lt;/P&gt;&lt;P&gt;The default routing option is that MSCAN module is connected internally to CANPHY.&lt;/P&gt;&lt;P&gt;In that case, you have to at least enable CANPHY by CPCR_CPE bit and initialize MSCAN module for communication over CAN.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You have also three other routing options (MODRR0):&lt;/P&gt;&lt;P&gt;0b000 Default setting: MSCAN connects to CANPHY, interface internal only&lt;/P&gt;&lt;P&gt;0b001 Direct control setting: CP0DR[CPDR1] connects to CPTXD, interface internal only&lt;/P&gt;&lt;P&gt;0b100 Probe setting: MSCAN connects to CANPHY, interface visible on 2 external pins&lt;/P&gt;&lt;P&gt;0b110 Conformance test setting: Interface opened and all 4 signals routed externally&lt;/P&gt;&lt;P&gt;See Figure 2-2. CAN Routing Options Illustration in S12ZVC RM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case of Conformance test setting, the MSCAN pins will be at PS2, PS3 pins and PANPHY pins will be at PS0, PS1 pins.&lt;/P&gt;&lt;P&gt;This way, you could drive MSCAN module and CANPHY independently.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: MODRR0 register could be written just once in normal, anytime in special mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Feb 2016 14:36:50 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2016-02-25T14:36:50Z</dc:date>
    <item>
      <title>MC9S12ZVCA192</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZVCA192/m-p/484285#M12052</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, we are using the MSCAN module for CAN driver development. Is it required to configure CAN physical to use the internal CAN transceiver available in the microcontroller?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Feb 2016 11:45:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZVCA192/m-p/484285#M12052</guid>
      <dc:creator>sumathikulkarni</dc:creator>
      <dc:date>2016-02-24T11:45:19Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S12ZVCA192</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZVCA192/m-p/484286#M12053</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sumathi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to apologize, but I am not sure with your question.&lt;/P&gt;&lt;P&gt;S12ZVC contains MSCAN module and CANPHY (CAN transceiver).&lt;/P&gt;&lt;P&gt;The default routing option is that MSCAN module is connected internally to CANPHY.&lt;/P&gt;&lt;P&gt;In that case, you have to at least enable CANPHY by CPCR_CPE bit and initialize MSCAN module for communication over CAN.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You have also three other routing options (MODRR0):&lt;/P&gt;&lt;P&gt;0b000 Default setting: MSCAN connects to CANPHY, interface internal only&lt;/P&gt;&lt;P&gt;0b001 Direct control setting: CP0DR[CPDR1] connects to CPTXD, interface internal only&lt;/P&gt;&lt;P&gt;0b100 Probe setting: MSCAN connects to CANPHY, interface visible on 2 external pins&lt;/P&gt;&lt;P&gt;0b110 Conformance test setting: Interface opened and all 4 signals routed externally&lt;/P&gt;&lt;P&gt;See Figure 2-2. CAN Routing Options Illustration in S12ZVC RM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case of Conformance test setting, the MSCAN pins will be at PS2, PS3 pins and PANPHY pins will be at PS0, PS1 pins.&lt;/P&gt;&lt;P&gt;This way, you could drive MSCAN module and CANPHY independently.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: MODRR0 register could be written just once in normal, anytime in special mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Feb 2016 14:36:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZVCA192/m-p/484286#M12053</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2016-02-25T14:36:50Z</dc:date>
    </item>
  </channel>
</rss>