<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How use pierce oscillator on µc MC9S12A128CPV ? in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-use-pierce-oscillator-on-%C2%B5c-MC9S12A128CPV/m-p/481680#M12028</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erwan,&lt;/P&gt;&lt;P&gt;I suppose that this thread is related to your next thread:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/391931"&gt;https://community.freescale.com/thread/391931&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, MC9S12A128CPVE should work with the oscillator in Pierce mode.&lt;/P&gt;&lt;P&gt;In that case, the XCLKS=PE7 pin has to be connected (pulled-down) to GND.&lt;/P&gt;&lt;P&gt;I would like to recommend additional parallel resistor to crystal – for example, 1MOhm. However, this will be probably not the root cause.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The crystal circuit parts parameters should be evaluated with crystal manufacturer. But 22pF looks OK for most of the standard crystals.&lt;/P&gt;&lt;P&gt;Note: Crystal must be fundamental and not overtone.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please share your schematic with MCU surroundings that we could shortly check for any obvious or potential issues?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check power supply pins according to Table 2-2 MC9S12DT128 Power and Ground Connection Summary in RM:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/files/microcontrollers/doc/data_sheet/9S12DT128_ZIP.zip"&gt;http://www.nxp.com/files/microcontrollers/doc/data_sheet/9S12DT128_ZIP.zip&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check also chip orientation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 May 2016 12:58:14 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2016-05-12T12:58:14Z</dc:date>
    <item>
      <title>How use pierce oscillator on µc MC9S12A128CPV ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-use-pierce-oscillator-on-%C2%B5c-MC9S12A128CPV/m-p/481679#M12027</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use 16MHz quartz with 22pFfor each capacitor (cf schematic in attached) &lt;/P&gt;&lt;P&gt;But I've no frequency on the EXTAL pin.&lt;/P&gt;&lt;P&gt;May be I did something wrong ?&lt;/P&gt;&lt;P&gt;need help please.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2016 15:17:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-use-pierce-oscillator-on-%C2%B5c-MC9S12A128CPV/m-p/481679#M12027</guid>
      <dc:creator>erwancoton</dc:creator>
      <dc:date>2016-04-27T15:17:00Z</dc:date>
    </item>
    <item>
      <title>Re: How use pierce oscillator on µc MC9S12A128CPV ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-use-pierce-oscillator-on-%C2%B5c-MC9S12A128CPV/m-p/481680#M12028</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erwan,&lt;/P&gt;&lt;P&gt;I suppose that this thread is related to your next thread:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/391931"&gt;https://community.freescale.com/thread/391931&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, MC9S12A128CPVE should work with the oscillator in Pierce mode.&lt;/P&gt;&lt;P&gt;In that case, the XCLKS=PE7 pin has to be connected (pulled-down) to GND.&lt;/P&gt;&lt;P&gt;I would like to recommend additional parallel resistor to crystal – for example, 1MOhm. However, this will be probably not the root cause.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The crystal circuit parts parameters should be evaluated with crystal manufacturer. But 22pF looks OK for most of the standard crystals.&lt;/P&gt;&lt;P&gt;Note: Crystal must be fundamental and not overtone.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please share your schematic with MCU surroundings that we could shortly check for any obvious or potential issues?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check power supply pins according to Table 2-2 MC9S12DT128 Power and Ground Connection Summary in RM:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/files/microcontrollers/doc/data_sheet/9S12DT128_ZIP.zip"&gt;http://www.nxp.com/files/microcontrollers/doc/data_sheet/9S12DT128_ZIP.zip&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check also chip orientation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 May 2016 12:58:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-use-pierce-oscillator-on-%C2%B5c-MC9S12A128CPV/m-p/481680#M12028</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2016-05-12T12:58:14Z</dc:date>
    </item>
    <item>
      <title>Re: How use pierce oscillator on µc MC9S12A128CPV ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-use-pierce-oscillator-on-%C2%B5c-MC9S12A128CPV/m-p/481681#M12029</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi radeks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, it’s ok with 1M in parallel on the crystal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a good day&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erwan &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;De : RadekS  &lt;/P&gt;&lt;P&gt;Envoyé : jeudi 12 mai 2016 14:59&lt;/P&gt;&lt;P&gt;À : Erwan Coton &amp;lt;ecoton@lea-photonics.com&amp;gt;&lt;/P&gt;&lt;P&gt;Objet : Re:  - How use pierce oscillator on µc MC9S12A128CPV ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &amp;lt;https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg&amp;gt; NXP Community &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How use pierce oscillator on µc MC9S12A128CPV ? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reply from Radek Sestak &amp;lt;https://community.freescale.com/people/RadekS?et=watches.email.thread&amp;gt;  in S12 / MagniV Microcontrollers - View the full discussion &amp;lt;https://community.freescale.com/message/644481?et=watches.email.thread#comment-644481&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 May 2016 16:16:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-use-pierce-oscillator-on-%C2%B5c-MC9S12A128CPV/m-p/481681#M12029</guid>
      <dc:creator>erwancoton</dc:creator>
      <dc:date>2016-05-12T16:16:23Z</dc:date>
    </item>
  </channel>
</rss>