<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Fraction data convert to Float in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Fraction-data-convert-to-Float/m-p/480676#M12011</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ahn,&lt;/P&gt;&lt;P&gt;As correctly mentioned by Edward:&lt;/P&gt;&lt;P&gt;We should divide 32-bit fixed point number in format Q1.31 by 0x80000000 for getting signed fractional [-1,1) number.&lt;/P&gt;&lt;P&gt;FRAC32() is defined in SWLIBS_Defines.h file as:&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="_jivemacro_uid_14600209600905537 jive_macro_code jive_text_macro" data-renderedposition="112_8_1192_48" jivemacro_uid="_14600209600905537"&gt;&lt;P&gt;/*! Macro converting a signed fractional [-1,1) number into a 32-bit fixed point number in format Q1.31.*/&lt;/P&gt;&lt;P&gt;#define FRAC32(x) ((tFrac32) ((x &amp;lt; FRACT_MAX) ? ((x &amp;gt;= FRACT_MIN) ? (x*2147483648.0) : INT32_MIN) : INT32_MAX))&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;Note: 2147483648=0x80000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since tFrac32 type = tS32 type = signed long type (according SWLIBS_Typedefs.h), we do not need to test sign in this case and command&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_macro_code jive_text_macro _jivemacro_uid_14600209900841739" data-renderedposition="238_8_1192_32" jivemacro_uid="_14600209900841739"&gt;&lt;P&gt;float f = (float)x / 0x80000000;&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;should work correctly also for negative numbers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Code&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_macro_code _jivemacro_uid_14600209686783149 jive_text_macro" data-renderedposition="348_8_1192_80" jivemacro_uid="_14600209686783149"&gt;&lt;P&gt;if( x &amp;amp; 0x8000000) // is it negative&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; f = - ( (float)(0-x) / 0x80000000 );&lt;/P&gt;&lt;P&gt;else&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; f = (float)x / 0x80000000 ;&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;is necessary when input data x are unsigned type.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Apr 2016 09:23:55 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2016-04-07T09:23:55Z</dc:date>
    <item>
      <title>Fraction data convert to Float</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Fraction-data-convert-to-Float/m-p/480674#M12009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Fraction data convert to Float &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have result fraction data format with below Math_Lib &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But that is the data type difficult show to me &lt;/P&gt;&lt;P&gt;So, i want to show "0x10000000(FRAC32)" --&amp;gt; "0.125"&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can i do? &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#include "mlib.h"&lt;/P&gt;&lt;P&gt;tFrac32 f32In1;&lt;/P&gt;&lt;P&gt;tFrac32 f32In2;&lt;/P&gt;&lt;P&gt;tFrac32 f32Out;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Function MLIB_Mul_F32&lt;/P&gt;&lt;P&gt;Automotive Math and Motor Control Library Set for Carcassonne MC9S12ZVM devices, Rev. 8&lt;/P&gt;&lt;P&gt;450 Freescale Semiconductor, Inc.&lt;/P&gt;&lt;P&gt;void main(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;// first input = 0.5&lt;/P&gt;&lt;P&gt;f32In1 = FRAC32 (0.5);&lt;/P&gt;&lt;P&gt;// second input = 0.25&lt;/P&gt;&lt;P&gt;f32In2 = FRAC32 (0.25);&lt;/P&gt;&lt;P&gt;// output should be 0x10000000 = FRAC32(0.125)&lt;/P&gt;&lt;P&gt;f32Out = MLIB_Mul_F32(f32In1,f32In2);&lt;/P&gt;&lt;P&gt;// output should be 0x10000000 = FRAC32(0.125)&lt;/P&gt;&lt;P&gt;f32Out = MLIB_Mul (f32In1,f32In2,F32);&lt;/P&gt;&lt;P&gt;// ##############################################################&lt;/P&gt;&lt;P&gt;// Available only if 32-bit fractional implementation selected&lt;/P&gt;&lt;P&gt;// as default&lt;/P&gt;&lt;P&gt;// ##############################################################&lt;/P&gt;&lt;P&gt;// output should be 0x10000000 = FRAC32(0.125)&lt;/P&gt;&lt;P&gt;f32Out = MLIB_Mul (f32In1,f32In2);&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 10:36:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Fraction-data-convert-to-Float/m-p/480674#M12009</guid>
      <dc:creator>ahnjoseph</dc:creator>
      <dc:date>2016-04-05T10:36:00Z</dc:date>
    </item>
    <item>
      <title>Re: Fraction data convert to Float</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Fraction-data-convert-to-Float/m-p/480675#M12010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;0x10000000 / 0x80000000 = 0.125, so for unsigned fractions conversion could look like this&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;float f = (float)x / 0x80000000 ;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Signed:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if( x &amp;amp; 0x8000000) // is it negative&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; f = - ( (float)(0-x) / 0x80000000 );&lt;/P&gt;&lt;P&gt;else&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; f = (float)x / 0x80000000 ;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 13:34:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Fraction-data-convert-to-Float/m-p/480675#M12010</guid>
      <dc:creator>kef2</dc:creator>
      <dc:date>2016-04-05T13:34:37Z</dc:date>
    </item>
    <item>
      <title>Re: Fraction data convert to Float</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Fraction-data-convert-to-Float/m-p/480676#M12011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ahn,&lt;/P&gt;&lt;P&gt;As correctly mentioned by Edward:&lt;/P&gt;&lt;P&gt;We should divide 32-bit fixed point number in format Q1.31 by 0x80000000 for getting signed fractional [-1,1) number.&lt;/P&gt;&lt;P&gt;FRAC32() is defined in SWLIBS_Defines.h file as:&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="_jivemacro_uid_14600209600905537 jive_macro_code jive_text_macro" data-renderedposition="112_8_1192_48" jivemacro_uid="_14600209600905537"&gt;&lt;P&gt;/*! Macro converting a signed fractional [-1,1) number into a 32-bit fixed point number in format Q1.31.*/&lt;/P&gt;&lt;P&gt;#define FRAC32(x) ((tFrac32) ((x &amp;lt; FRACT_MAX) ? ((x &amp;gt;= FRACT_MIN) ? (x*2147483648.0) : INT32_MIN) : INT32_MAX))&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;Note: 2147483648=0x80000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since tFrac32 type = tS32 type = signed long type (according SWLIBS_Typedefs.h), we do not need to test sign in this case and command&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_macro_code jive_text_macro _jivemacro_uid_14600209900841739" data-renderedposition="238_8_1192_32" jivemacro_uid="_14600209900841739"&gt;&lt;P&gt;float f = (float)x / 0x80000000;&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;should work correctly also for negative numbers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Code&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_macro_code _jivemacro_uid_14600209686783149 jive_text_macro" data-renderedposition="348_8_1192_80" jivemacro_uid="_14600209686783149"&gt;&lt;P&gt;if( x &amp;amp; 0x8000000) // is it negative&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; f = - ( (float)(0-x) / 0x80000000 );&lt;/P&gt;&lt;P&gt;else&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; f = (float)x / 0x80000000 ;&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;is necessary when input data x are unsigned type.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Apr 2016 09:23:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Fraction-data-convert-to-Float/m-p/480676#M12011</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2016-04-07T09:23:55Z</dc:date>
    </item>
  </channel>
</rss>