<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: power on reset pin status</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/power-on-reset-pin-status/m-p/480491#M11999</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much for the reply. It feels great that now a days we get reply in very short duration. Sorry that i did not mention my micro it is S12xE family. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Feb 2016 15:44:40 GMT</pubDate>
    <dc:creator>rahulkrishna</dc:creator>
    <dc:date>2016-02-24T15:44:40Z</dc:date>
    <item>
      <title>power on reset pin status</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/power-on-reset-pin-status/m-p/480489#M11997</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi I am facing a very difficult problem, I have given one of the port J port to control an output pin. So when required i will give either 1 or 0 based on requirement. The problem i am facing is on power on reset this pin is a high and my output is going high. when the control comes to maintain i am able to initialize. Please advice me how to control this pin so that on power on or reset i can make it a low. I am using S12x.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Feb 2016 13:47:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/power-on-reset-pin-status/m-p/480489#M11997</guid>
      <dc:creator>rahulkrishna</dc:creator>
      <dc:date>2016-02-23T13:47:19Z</dc:date>
    </item>
    <item>
      <title>Re: power on reset pin status</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/power-on-reset-pin-status/m-p/480490#M11998</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi rahul,&lt;/P&gt;&lt;P&gt;I suppose for now that you use MCU from S12XD Family.&lt;/P&gt;&lt;P&gt;The default status of port J pins is digital input with enabled internal pull-up after reset.&lt;/P&gt;&lt;P&gt;Please look at Table 1-7. Signal Properties Summary in RM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I could see two basic possible solutions:&lt;/P&gt;&lt;P&gt;1.&amp;nbsp;&amp;nbsp;&amp;nbsp; You could select different pin for driving that external circuit. In that case, you could choose pins with default pull-down (no such pins for S12XD family) or pins with default disabled pull-device (port A, B, C, D, H, M, P, T, AD). When we select pin with default disabled pull-device after reset, we should use external pull-down for ensure that voltage level will stay low until we configure this pins as outputs.&lt;/P&gt;&lt;P&gt;2.&amp;nbsp;&amp;nbsp;&amp;nbsp; Internal pull-device is weak. We could assume that internal pull-up value is higher than 25kOhm. In that case, we could use external strong pull down (for example 2.2kOhm) at port J for ensure that that voltage level will stay low (below 0.8V) until we configure this pins as output.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Feb 2016 17:54:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/power-on-reset-pin-status/m-p/480490#M11998</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2016-02-23T17:54:44Z</dc:date>
    </item>
    <item>
      <title>Re: power on reset pin status</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/power-on-reset-pin-status/m-p/480491#M11999</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much for the reply. It feels great that now a days we get reply in very short duration. Sorry that i did not mention my micro it is S12xE family. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Feb 2016 15:44:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/power-on-reset-pin-status/m-p/480491#M11999</guid>
      <dc:creator>rahulkrishna</dc:creator>
      <dc:date>2016-02-24T15:44:40Z</dc:date>
    </item>
  </channel>
</rss>