<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: Ways to Soft reset S12ZVC controller</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Ways-to-Soft-reset-S12ZVC-controller/m-p/474758#M11924</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is that normal mode and special mode in COP. is it w.r.t COP or MCU modes. How to configure special mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Dec 2015 04:22:37 GMT</pubDate>
    <dc:creator>kiranbhat</dc:creator>
    <dc:date>2015-12-22T04:22:37Z</dc:date>
    <item>
      <title>Ways to Soft reset S12ZVC controller</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Ways-to-Soft-reset-S12ZVC-controller/m-p/474756#M11922</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Is there any assembly instruction to reset the controller through code???? if yes any sample code can be available.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Dec 2015 07:26:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Ways-to-Soft-reset-S12ZVC-controller/m-p/474756#M11922</guid>
      <dc:creator>kiranbhat</dc:creator>
      <dc:date>2015-12-10T07:26:21Z</dc:date>
    </item>
    <item>
      <title>Re: Ways to Soft reset S12ZVC controller</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Ways-to-Soft-reset-S12ZVC-controller/m-p/474757#M11923</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.0pt;"&gt;Hi kiran,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.0pt;"&gt;Simplest way is using COP watchdog.&lt;/SPAN&gt;&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;&lt;SPAN style="font-size: 9.0pt;"&gt;Initialize COP watchdog by write into CPMUCOP register. For example: CPMUCOP=0x01;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="font-size: 9.0pt;"&gt;Trigger MCU reset by write into CPMUCRMCOP register (any value other than 0x55 or 0xAA). For example:&amp;nbsp; CPMUCRMCOP=0x00;&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.0pt;"&gt;Note: bits in CPMUCOP could be written just once in Normal mode. Please ensure that your code do not initialize CPMUCOP register by write zeros prior requested initialization (step 1) - Writing CR[2:0] to “000” has no effect, but counts for the “write once” condition.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Dec 2015 14:39:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Ways-to-Soft-reset-S12ZVC-controller/m-p/474757#M11923</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2015-12-15T14:39:36Z</dc:date>
    </item>
    <item>
      <title>Re: Ways to Soft reset S12ZVC controller</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Ways-to-Soft-reset-S12ZVC-controller/m-p/474758#M11924</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is that normal mode and special mode in COP. is it w.r.t COP or MCU modes. How to configure special mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Dec 2015 04:22:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Ways-to-Soft-reset-S12ZVC-controller/m-p/474758#M11924</guid>
      <dc:creator>kiranbhat</dc:creator>
      <dc:date>2015-12-22T04:22:37Z</dc:date>
    </item>
    <item>
      <title>Re: Ways to Soft reset S12ZVC controller</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Ways-to-Soft-reset-S12ZVC-controller/m-p/474759#M11925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi kiran,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;The BKGD/MODC signal is used as a MCU operating mode select during reset. The state of this signal is latched to the MODC bit at the rising edge of RESET.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;If BKGD signal is high during reset, MCU will start in Normal single chip mode – CPU will start execute user code.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;If BKGD signal is low during reset, MCU will start in Special single chip mode – CPU waits for BDM commands.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Please see chapter 1.10.1 Chip Configuration Modes in RM for more details.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;For simplicity, special mode is used for debugging, normal mode for run code without debugger.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Dec 2015 22:35:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Ways-to-Soft-reset-S12ZVC-controller/m-p/474759#M11925</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2015-12-29T22:35:42Z</dc:date>
    </item>
    <item>
      <title>Re: Ways to Soft reset S12ZVC controller</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Ways-to-Soft-reset-S12ZVC-controller/m-p/474760#M11926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The COP reset is not a soft reset, but a hard reset! For soft reset jump to application start:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;SPAN style="font-family: courier new,courier,monospace;"&gt;asm jmp _Startup;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 May 2017 08:55:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Ways-to-Soft-reset-S12ZVC-controller/m-p/474760#M11926</guid>
      <dc:creator>niba</dc:creator>
      <dc:date>2017-05-10T08:55:50Z</dc:date>
    </item>
  </channel>
</rss>