<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Update Firmware EVB Board in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Update-Firmware-EVB-Board/m-p/472198#M11905</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Thorsten,&lt;/P&gt;&lt;P&gt;OSBDM has to be enumerated as bootloader for the firmware update.&lt;/P&gt;&lt;P&gt;So, please disconnect USB cable, insert jumper, reconnect USB cable, wait until drivers are installed (it could take some time for the first time) and after that click on OK.&lt;/P&gt;&lt;P&gt;After the firmware update, please disconnect USB cable, remove the jumper, reconnect USB cable, wait until drivers are installed (it could take some time for the first time) and after that click on OK.&lt;/P&gt;&lt;P&gt;With that, OSBDM should be up updated and the debugger will continue in loading code into MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If this will not work, please go to link:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/OSBDM/"&gt;http://www.pemicro.com/OSBDM/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;You could download here OSBDM firmware with firmware updater tool (standalone tool for updating OSBDM and other PEmicro tools firmware).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Mar 2016 09:26:56 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2016-03-14T09:26:56Z</dc:date>
    <item>
      <title>Update Firmware EVB Board</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Update-Firmware-EVB-Board/m-p/472196#M11903</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, i get the massage the OSJATG firmware ist old, set the jumper for update. I try it but it dosent work.&lt;/P&gt;&lt;P&gt;The picture shows the Message and the other in yellow the jumper setting. Whats me mistake?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Mar 2016 11:32:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Update-Firmware-EVB-Board/m-p/472196#M11903</guid>
      <dc:creator>thorstenmulun</dc:creator>
      <dc:date>2016-03-12T11:32:03Z</dc:date>
    </item>
    <item>
      <title>Re: Update Firmware EVB Board</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Update-Firmware-EVB-Board/m-p/472197#M11904</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;You only need set the jumper to J36, then click ok .&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22734i78D5AC6D885C5EB4/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If it still can not work , please take a screenshot about the&lt;/P&gt;&lt;P&gt;phenomenons step by step.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice Yang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Mar 2016 05:28:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Update-Firmware-EVB-Board/m-p/472197#M11904</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-03-14T05:28:01Z</dc:date>
    </item>
    <item>
      <title>Re: Update Firmware EVB Board</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Update-Firmware-EVB-Board/m-p/472198#M11905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Thorsten,&lt;/P&gt;&lt;P&gt;OSBDM has to be enumerated as bootloader for the firmware update.&lt;/P&gt;&lt;P&gt;So, please disconnect USB cable, insert jumper, reconnect USB cable, wait until drivers are installed (it could take some time for the first time) and after that click on OK.&lt;/P&gt;&lt;P&gt;After the firmware update, please disconnect USB cable, remove the jumper, reconnect USB cable, wait until drivers are installed (it could take some time for the first time) and after that click on OK.&lt;/P&gt;&lt;P&gt;With that, OSBDM should be up updated and the debugger will continue in loading code into MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If this will not work, please go to link:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/OSBDM/"&gt;http://www.pemicro.com/OSBDM/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;You could download here OSBDM firmware with firmware updater tool (standalone tool for updating OSBDM and other PEmicro tools firmware).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Mar 2016 09:26:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Update-Firmware-EVB-Board/m-p/472198#M11905</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2016-03-14T09:26:56Z</dc:date>
    </item>
  </channel>
</rss>