<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: Some issue during using P&amp;E USE multilink interface debug MS9S12VR</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Some-issue-during-using-P-E-USE-multilink-interface-debug/m-p/471557#M11893</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Juejie,&lt;/P&gt;&lt;P&gt;It seems that BDM communication is not correct in your case.&lt;/P&gt;&lt;P&gt;Unfortunately, I was not able to reproduce it.&lt;/P&gt;&lt;P&gt;From my point of view, it looks like that there start some communication, but it fails very early.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Typical issues:&lt;/P&gt;&lt;P&gt;1.&amp;nbsp;&amp;nbsp;&amp;nbsp; Please check BDM connector orientation&lt;/P&gt;&lt;P&gt;2.&amp;nbsp;&amp;nbsp;&amp;nbsp; Please connect just one BDM interface to your PC&lt;/P&gt;&lt;P&gt;3.&amp;nbsp;&amp;nbsp;&amp;nbsp; S12VR needs battery voltage, please connect 12V to your board&lt;/P&gt;&lt;P&gt;4.&amp;nbsp;&amp;nbsp;&amp;nbsp; Do you use external watchdog? Please disconnect it during programming.&lt;/P&gt;&lt;P&gt;5.&amp;nbsp;&amp;nbsp;&amp;nbsp; Please check ribbon cable connection. The cable or one of the connectors may be broken.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you use any evaluation board, or you have your own PCB?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The strange is also your missing line prior “MCU clock speed:” and block module ranges. There should be line with loading flash parameters. So, the problem may be also in some wrong project path settings.&lt;/P&gt;&lt;P&gt;In my case it looks like:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/58933iA93744E1642F97B5/image-size/large?v=v2&amp;amp;px=999" title="hiwave-log.png" alt="hiwave-log.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In case of CW5.2 is there line:&lt;/P&gt;&lt;P&gt;FP: FLASH parameters loaded for MC9S12VR64_V0_5(NVMIF2 rev 3,3,3,3) from C:\Program Files (x86)\Freescale\CWS12v5.2\prog\FPP\mcu01CD.fpp&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: 5.9 version of IDE (it is common for several CW versions). Please look at menu-Help-About-Installed Products for more details about CW version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 May 2016 14:47:29 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2016-05-16T14:47:29Z</dc:date>
    <item>
      <title>Some issue during using P&amp;E USE multilink interface debug MS9S12VR</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Some-issue-during-using-P-E-USE-multilink-interface-debug/m-p/471556#M11892</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;IDE is codewarrior 5.9.&lt;/P&gt;&lt;P&gt;When i actiave the debug, during program flash the tool always report following error.&lt;/P&gt;&lt;P&gt;Can some one help to explain the root cause?&lt;/P&gt;&lt;P&gt;I double confirm the VDD and GND is working ok. &lt;/P&gt;&lt;P&gt;Is there a issue the MCU clock speed is 5000Hz?&lt;/P&gt;&lt;P&gt;Thanks very much!&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/121594iA621D8147C1A4EF0/image-size/large?v=v2&amp;amp;px=999" title="149399_149399.png" alt="149399_149399.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/57697i132D16EC6BF5B55A/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 15 May 2016 14:12:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Some-issue-during-using-P-E-USE-multilink-interface-debug/m-p/471556#M11892</guid>
      <dc:creator>kernwang</dc:creator>
      <dc:date>2016-05-15T14:12:24Z</dc:date>
    </item>
    <item>
      <title>Re: Some issue during using P&amp;E USE multilink interface debug MS9S12VR</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Some-issue-during-using-P-E-USE-multilink-interface-debug/m-p/471557#M11893</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Juejie,&lt;/P&gt;&lt;P&gt;It seems that BDM communication is not correct in your case.&lt;/P&gt;&lt;P&gt;Unfortunately, I was not able to reproduce it.&lt;/P&gt;&lt;P&gt;From my point of view, it looks like that there start some communication, but it fails very early.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Typical issues:&lt;/P&gt;&lt;P&gt;1.&amp;nbsp;&amp;nbsp;&amp;nbsp; Please check BDM connector orientation&lt;/P&gt;&lt;P&gt;2.&amp;nbsp;&amp;nbsp;&amp;nbsp; Please connect just one BDM interface to your PC&lt;/P&gt;&lt;P&gt;3.&amp;nbsp;&amp;nbsp;&amp;nbsp; S12VR needs battery voltage, please connect 12V to your board&lt;/P&gt;&lt;P&gt;4.&amp;nbsp;&amp;nbsp;&amp;nbsp; Do you use external watchdog? Please disconnect it during programming.&lt;/P&gt;&lt;P&gt;5.&amp;nbsp;&amp;nbsp;&amp;nbsp; Please check ribbon cable connection. The cable or one of the connectors may be broken.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you use any evaluation board, or you have your own PCB?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The strange is also your missing line prior “MCU clock speed:” and block module ranges. There should be line with loading flash parameters. So, the problem may be also in some wrong project path settings.&lt;/P&gt;&lt;P&gt;In my case it looks like:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/58933iA93744E1642F97B5/image-size/large?v=v2&amp;amp;px=999" title="hiwave-log.png" alt="hiwave-log.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In case of CW5.2 is there line:&lt;/P&gt;&lt;P&gt;FP: FLASH parameters loaded for MC9S12VR64_V0_5(NVMIF2 rev 3,3,3,3) from C:\Program Files (x86)\Freescale\CWS12v5.2\prog\FPP\mcu01CD.fpp&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: 5.9 version of IDE (it is common for several CW versions). Please look at menu-Help-About-Installed Products for more details about CW version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 May 2016 14:47:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Some-issue-during-using-P-E-USE-multilink-interface-debug/m-p/471557#M11893</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2016-05-16T14:47:29Z</dc:date>
    </item>
  </channel>
</rss>