<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: BDM connection problem with mc9s12c32 in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/BDM-connection-problem-with-mc9s12c32/m-p/452670#M11589</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sonal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately it is hard to say what could be reason for that behavior.&lt;/P&gt;&lt;P&gt;I would like to recommend double check connection on both sides of BDM ribbon cable.&lt;/P&gt;&lt;P&gt;Pin1=BKGD, pin2=GND, pin4=RESET, pin6=VCC.&lt;/P&gt;&lt;P&gt;The same has to be checked also on your board schematic/layout. Please be careful with top and bottom connector orientation…&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to recommend also try different power supply adapter with higher current capability.&lt;/P&gt;&lt;P&gt;BDM connection to MCU typically means increasing of power supply consumption (in mA range).&lt;/P&gt;&lt;P&gt;Is it possible measure board power supply current with and without BDM connected?&lt;/P&gt;&lt;P&gt;If you use laboratory power supply, are you sure that current limiter do not influence result voltage?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could try also different AC plugs. I already meet with situation where ground currents between two power sources cause problems during programming…&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could try different PC or BDM Multilink for at least localize source of that issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Sep 2015 09:20:35 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2015-09-17T09:20:35Z</dc:date>
    <item>
      <title>BDM connection problem with mc9s12c32</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/BDM-connection-problem-with-mc9s12c32/m-p/452669#M11588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;I am also facing same kind of problem with my new multilink universal programmer version C.&amp;nbsp; All voltages on micro-controller boards are ok. when i am connecting BDM blue light turning on.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After connecting to target orange light also turns on. ( connection happens) But when i am connecting BDM programmer input voltage drops .(i/p voltage= 10 V, after connectingBDM programmer power supply getting into CC mode from CV mode, and power supply voltage drops to 2.5V), by default VCC (5V) also drops.( i think there must be some short circuit happening, but dont know where exactly). I tried all things on my controller board. But facing same thing.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What can be the problem???&amp;nbsp; &lt;/P&gt;&lt;P&gt;Any solution?&amp;nbsp; &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; regards,&lt;/P&gt;&lt;P&gt;Sonal.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Sep 2015 05:43:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/BDM-connection-problem-with-mc9s12c32/m-p/452669#M11588</guid>
      <dc:creator>sonalchirme</dc:creator>
      <dc:date>2015-09-16T05:43:39Z</dc:date>
    </item>
    <item>
      <title>Re: BDM connection problem with mc9s12c32</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/BDM-connection-problem-with-mc9s12c32/m-p/452670#M11589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sonal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately it is hard to say what could be reason for that behavior.&lt;/P&gt;&lt;P&gt;I would like to recommend double check connection on both sides of BDM ribbon cable.&lt;/P&gt;&lt;P&gt;Pin1=BKGD, pin2=GND, pin4=RESET, pin6=VCC.&lt;/P&gt;&lt;P&gt;The same has to be checked also on your board schematic/layout. Please be careful with top and bottom connector orientation…&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to recommend also try different power supply adapter with higher current capability.&lt;/P&gt;&lt;P&gt;BDM connection to MCU typically means increasing of power supply consumption (in mA range).&lt;/P&gt;&lt;P&gt;Is it possible measure board power supply current with and without BDM connected?&lt;/P&gt;&lt;P&gt;If you use laboratory power supply, are you sure that current limiter do not influence result voltage?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could try also different AC plugs. I already meet with situation where ground currents between two power sources cause problems during programming…&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could try different PC or BDM Multilink for at least localize source of that issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Sep 2015 09:20:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/BDM-connection-problem-with-mc9s12c32/m-p/452670#M11589</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2015-09-17T09:20:35Z</dc:date>
    </item>
    <item>
      <title>Re: BDM connection problem with mc9s12c32</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/BDM-connection-problem-with-mc9s12c32/m-p/452671#M11590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey RadekS,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You rock man...:smileyhappy:&lt;/P&gt;&lt;P&gt;You are great..your suggestion is very accurate........&lt;/P&gt;&lt;P&gt;I solved this problem before your reply....&lt;/P&gt;&lt;P&gt; Input current was problem...&lt;/P&gt;&lt;P&gt;I set it littlebit high and problem got solved...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks you...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Sep 2015 16:03:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/BDM-connection-problem-with-mc9s12c32/m-p/452671#M11590</guid>
      <dc:creator>sonalchirme</dc:creator>
      <dc:date>2015-09-17T16:03:05Z</dc:date>
    </item>
    <item>
      <title>Re: BDM connection problem with mc9s12c32</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/BDM-connection-problem-with-mc9s12c32/m-p/452672#M11591</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sonal,&lt;/P&gt;&lt;P&gt;You're welcome.&lt;/P&gt;&lt;P&gt;I am glad that the problem has been resolved.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wish you good luck in the future development.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Sep 2015 06:53:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/BDM-connection-problem-with-mc9s12c32/m-p/452672#M11591</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2015-09-18T06:53:10Z</dc:date>
    </item>
  </channel>
</rss>