<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックDual S12x Communication</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Dual-S12x-Communication/m-p/452589#M11585</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am thinking of a new product that uses two S12XE. One MCU will be a slave and read sensors. The main MCU would either request the information from the slave or receive it when is ready. I have done this in the past using SCI. I am looking at using CAN Bus to communicate.&amp;nbsp; Do I still need CAN transceivers, or can I just connect the low level signals from the CAN pins.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am open to ideas using some other method.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ray.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Aug 2015 03:12:20 GMT</pubDate>
    <dc:creator>rayhall</dc:creator>
    <dc:date>2015-08-20T03:12:20Z</dc:date>
    <item>
      <title>Dual S12x Communication</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Dual-S12x-Communication/m-p/452589#M11585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am thinking of a new product that uses two S12XE. One MCU will be a slave and read sensors. The main MCU would either request the information from the slave or receive it when is ready. I have done this in the past using SCI. I am looking at using CAN Bus to communicate.&amp;nbsp; Do I still need CAN transceivers, or can I just connect the low level signals from the CAN pins.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am open to ideas using some other method.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ray.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2015 03:12:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Dual-S12x-Communication/m-p/452589#M11585</guid>
      <dc:creator>rayhall</dc:creator>
      <dc:date>2015-08-20T03:12:20Z</dc:date>
    </item>
    <item>
      <title>Re: Dual S12x Communication</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Dual-S12x-Communication/m-p/452590#M11586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A href="http://electronics.stackexchange.com/questions/30564/is-a-can-enabled-microcontroller-sufficient-to-drive-a-can-bus" title="http://electronics.stackexchange.com/questions/30564/is-a-can-enabled-microcontroller-sufficient-to-drive-a-can-bus"&gt;Is a CAN enabled microcontroller sufficient to drive a CAN bus? - Electrical Engineering Stack Exchange&lt;/A&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2015 06:09:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Dual-S12x-Communication/m-p/452590#M11586</guid>
      <dc:creator>kef2</dc:creator>
      <dc:date>2015-08-20T06:09:37Z</dc:date>
    </item>
    <item>
      <title>Re: Dual S12x Communication</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Dual-S12x-Communication/m-p/452591#M11587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ray,&lt;/P&gt;&lt;P&gt;Edward is right.&lt;/P&gt;&lt;P&gt;You don’t need transceivers. For short length communication, diodes and pull-up are sufficient solution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is simply scheme for connection of four CAN modules together at DEMO9S12XEP100 board as inspiration for you:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52595i72E4955B375E317F/image-size/large?v=v2&amp;amp;px=999" title="CAN without transceiver DemoXEP100.bmp" alt="CAN without transceiver DemoXEP100.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Tested and proved.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2015 09:20:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Dual-S12x-Communication/m-p/452591#M11587</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2015-08-20T09:20:34Z</dc:date>
    </item>
  </channel>
</rss>