<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックExternal Interrupt of 9S12DP512</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/External-Interrupt-of-9S12DP512/m-p/435765#M11436</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;May I know how many external interrupt would S12DP512 have? Is It only one which called nXIRQ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;If I have need to have more than one external interrupt, should I need to change to use another model? &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;Any suggestion? Please help.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;Many thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Apr 2015 04:21:38 GMT</pubDate>
    <dc:creator>monstor</dc:creator>
    <dc:date>2015-04-23T04:21:38Z</dc:date>
    <item>
      <title>External Interrupt of 9S12DP512</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/External-Interrupt-of-9S12DP512/m-p/435765#M11436</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;May I know how many external interrupt would S12DP512 have? Is It only one which called nXIRQ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;If I have need to have more than one external interrupt, should I need to change to use another model? &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;Any suggestion? Please help.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;Many thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Apr 2015 04:21:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/External-Interrupt-of-9S12DP512/m-p/435765#M11436</guid>
      <dc:creator>monstor</dc:creator>
      <dc:date>2015-04-23T04:21:38Z</dc:date>
    </item>
    <item>
      <title>Re: External Interrupt of 9S12DP512</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/External-Interrupt-of-9S12DP512/m-p/435766#M11437</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There's a lot of external interrupt inputs. You didn't say whether you need level sensitive interrupt inputs, or edge sensitive interrupt inputs. Number of level sensitive int. inputs is small. There are two dedicated inputs, /IRQ and /XIRQ. But being creative, I think it is possible to use two SCI RxD inputs as level sensitive interrupts.. with some delay. Perhaps PWM emergency shutdown input can be used as level sensitive interrupt input, I'm not sure, please check documentation. Any way, using something like AND gates, or even chip diodes and one pull up resistor, you can easily multiply number of level sensitive interrupt inputs.&lt;/P&gt;&lt;P&gt;And speaking about edge sensitive interrupt inputs, you have many of them. See PORTJ, PORTH, PORTP interrupts. That's up to 8x3 edge sensitive interrupt inputs. There are also 8 timer input pins, which can be easily used as edge sensitive interrupt inputs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edward&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Apr 2015 06:54:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/External-Interrupt-of-9S12DP512/m-p/435766#M11437</guid>
      <dc:creator>kef2</dc:creator>
      <dc:date>2015-04-23T06:54:51Z</dc:date>
    </item>
    <item>
      <title>Re: External Interrupt of 9S12DP512</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/External-Interrupt-of-9S12DP512/m-p/435767#M11438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edward is right.&lt;/P&gt;&lt;P&gt;Here is the S12DP512 documentation pack download: &lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/microcontrollers/doc/data_sheet/9S12DP512_ZIP.zip?fasp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=zip&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.zip" title="http://cache.freescale.com/files/microcontrollers/doc/data_sheet/9S12DP512_ZIP.zip?fasp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=zip&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.zip"&gt;http://cache.freescale.com/files/microcontrollers/doc/data_sheet/9S12DP512_ZIP.zip&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Unzip it and then, in the 9S12DP512DGV1.pdf find Table 5-1 Interrupt Vector Locations. If you will use any of Port J/P/H pins, see S12DP256PIMV3.pdf document for correct configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;iggi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Apr 2015 09:11:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/External-Interrupt-of-9S12DP512/m-p/435767#M11438</guid>
      <dc:creator>iggi</dc:creator>
      <dc:date>2015-04-23T09:11:46Z</dc:date>
    </item>
  </channel>
</rss>