<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックTWR-S12G128 OSBDM Bootloader</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/TWR-S12G128-OSBDM-Bootloader/m-p/435010#M11434</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have found that the TWR-S12G128 Demostration board is loaded with a bootloader. The documentation for the board states this,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;The OSBDM is pre-programmed with a bootloader application to &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;allow field updates. The USB bootloader communicates with a &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;GUI application running on a host PC. The GUI application allows &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;the user to update OSBDM firmware easily and quickly. Option &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;jumper JP401 enables the bootloader at startup. This option &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;header is not populated in default configuration. Refer to &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Freescale Application Note AN3561 for details on using the &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;GUI application and bootloader. The application note may be &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;found at &lt;A href="https://community.nxp.com/www.freescale.com" target="test_blank"&gt;www.freescale.com&lt;/A&gt; or at &lt;A href="https://community.nxp.com/www.axman.com/support" target="test_blank"&gt;www.axman.com/support&lt;/A&gt;.&lt;/EM&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Where can I get a copy of this bootloader and the PC software used for the updates.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ray.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Aug 2015 01:49:26 GMT</pubDate>
    <dc:creator>rayhall</dc:creator>
    <dc:date>2015-08-13T01:49:26Z</dc:date>
    <item>
      <title>TWR-S12G128 OSBDM Bootloader</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/TWR-S12G128-OSBDM-Bootloader/m-p/435010#M11434</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have found that the TWR-S12G128 Demostration board is loaded with a bootloader. The documentation for the board states this,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;The OSBDM is pre-programmed with a bootloader application to &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;allow field updates. The USB bootloader communicates with a &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;GUI application running on a host PC. The GUI application allows &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;the user to update OSBDM firmware easily and quickly. Option &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;jumper JP401 enables the bootloader at startup. This option &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;header is not populated in default configuration. Refer to &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Freescale Application Note AN3561 for details on using the &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;GUI application and bootloader. The application note may be &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;found at &lt;A href="https://community.nxp.com/www.freescale.com" target="test_blank"&gt;www.freescale.com&lt;/A&gt; or at &lt;A href="https://community.nxp.com/www.axman.com/support" target="test_blank"&gt;www.axman.com/support&lt;/A&gt;.&lt;/EM&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Where can I get a copy of this bootloader and the PC software used for the updates.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ray.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Aug 2015 01:49:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/TWR-S12G128-OSBDM-Bootloader/m-p/435010#M11434</guid>
      <dc:creator>rayhall</dc:creator>
      <dc:date>2015-08-13T01:49:26Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-S12G128 OSBDM Bootloader</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/TWR-S12G128-OSBDM-Bootloader/m-p/435011#M11435</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ray,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;OSBDM product page:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/osbdm/"&gt;http://www.pemicro.com/osbdm/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could download Firmware updater, PE drivers, design documents,…&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: Firmware updater could be also used for updating firmware on other PEmicro debuggers like Multilink Universal (debugger for Freescale Kinetis, ColdFire V1/+V1, ColdFire V2-4, Qorivva 55xx/56xx, HCS08,&amp;nbsp; HC(S)12(X), RS08, and DSC microcontrollers). You have to change firmware prior programming different type of MCU - for example between e.g. Kinetis and S12.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Aug 2015 08:23:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/TWR-S12G128-OSBDM-Bootloader/m-p/435011#M11435</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2015-08-13T08:23:57Z</dc:date>
    </item>
  </channel>
</rss>