<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: mc9s12g128 100pin Config Unused Pin</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/mc9s12g128-100pin-Config-Unused-Pin/m-p/427729#M11351</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For lowest power consumption, please set unused pins as digital output or digital input with enabled internal pull-up or pull-down.&lt;/P&gt;&lt;P&gt;In general, you should avoid situation where digital pin will be in undefined state. Middle range voltage at digital input pin (e.g. 2.5V with 5V VCC) could cause unexpected power consumption.&lt;/P&gt;&lt;P&gt;This is not valid for analog pins until we enable digital input buffer. After that situation will be the same as in case of digital pins.&lt;/P&gt;&lt;P&gt;However we should connect unused analog pins to some defined voltage at least because immunity against noise.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;More details could be found for example here:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/files/microcontrollers/doc/app_note/AN2727.pdf"&gt;http://www.freescale.com/files/microcontrollers/doc/app_note/AN2727.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;or here:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/files/microcontrollers/doc/app_note/AN3262.pdf"&gt;http://www.freescale.com/files/microcontrollers/doc/app_note/AN3262.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Note: these application nodes was created for older MCUs (250nm technology), not all information are applicable also for S12G.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Jun 2015 13:20:00 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2015-06-19T13:20:00Z</dc:date>
    <item>
      <title>mc9s12g128 100pin Config Unused Pin</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/mc9s12g128-100pin-Config-Unused-Pin/m-p/427728#M11350</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When MCU is go to Full Stop Mode,because the PORTA(some pins are &lt;SPAN style="color: #e23d39;"&gt;configed output&lt;/SPAN&gt;) can not be configed &lt;SPAN style="color: #e23d39;"&gt;Pullup&lt;/SPAN&gt;,So the ununsed pin is configed &lt;SPAN style="color: #7ed529;"&gt;output and output 1&lt;/SPAN&gt;.Whether the&amp;nbsp; &lt;SPAN style="color: #7ed529;"&gt;power consumption&lt;/SPAN&gt; is lowermost?Please give me some suggestion,Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2015 09:31:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/mc9s12g128-100pin-Config-Unused-Pin/m-p/427728#M11350</guid>
      <dc:creator>张华荣</dc:creator>
      <dc:date>2015-06-04T09:31:15Z</dc:date>
    </item>
    <item>
      <title>Re: mc9s12g128 100pin Config Unused Pin</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/mc9s12g128-100pin-Config-Unused-Pin/m-p/427729#M11351</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For lowest power consumption, please set unused pins as digital output or digital input with enabled internal pull-up or pull-down.&lt;/P&gt;&lt;P&gt;In general, you should avoid situation where digital pin will be in undefined state. Middle range voltage at digital input pin (e.g. 2.5V with 5V VCC) could cause unexpected power consumption.&lt;/P&gt;&lt;P&gt;This is not valid for analog pins until we enable digital input buffer. After that situation will be the same as in case of digital pins.&lt;/P&gt;&lt;P&gt;However we should connect unused analog pins to some defined voltage at least because immunity against noise.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;More details could be found for example here:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/files/microcontrollers/doc/app_note/AN2727.pdf"&gt;http://www.freescale.com/files/microcontrollers/doc/app_note/AN2727.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;or here:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/files/microcontrollers/doc/app_note/AN3262.pdf"&gt;http://www.freescale.com/files/microcontrollers/doc/app_note/AN3262.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Note: these application nodes was created for older MCUs (250nm technology), not all information are applicable also for S12G.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jun 2015 13:20:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/mc9s12g128-100pin-Config-Unused-Pin/m-p/427729#M11351</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2015-06-19T13:20:00Z</dc:date>
    </item>
  </channel>
</rss>