<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: How can we set up a 64 - bit Integer operations under  CodeWarrior Development Studio for HCS12(X) Microcontrollers (Classic IDE) v5.1</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-we-set-up-a-64-bit-Integer-operations-under-CodeWarrior/m-p/404647#M11052</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's not true that 16bit MCU can't have 64bit integers in C. Even 8bit MCU's can do. But CW for S12(X) doesn't support it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Sep 2015 08:11:28 GMT</pubDate>
    <dc:creator>kef2</dc:creator>
    <dc:date>2015-09-14T08:11:28Z</dc:date>
    <item>
      <title>How can we set up a 64 - bit Integer operations under  CodeWarrior Development Studio for HCS12(X) Microcontrollers (Classic IDE) v5.1</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-we-set-up-a-64-bit-Integer-operations-under-CodeWarrior/m-p/404642#M11047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The customers is using CodeWarrior Development Studio for HCS12(X) Microcontrollers (Classic IDE) v5.1 do a S12 project，Which need use 64 bit integer operations. The results is correct when set unsigned long 32 bits, But if set to unsigned longlong 64 bits , the result is error. How can we set up a 64 - bit integer? thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Aug 2015 07:09:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-we-set-up-a-64-bit-Integer-operations-under-CodeWarrior/m-p/404642#M11047</guid>
      <dc:creator>xiuminsong</dc:creator>
      <dc:date>2015-08-28T07:09:59Z</dc:date>
    </item>
    <item>
      <title>Re: How can we set up a 64 - bit Integer operations under  CodeWarrior Development Studio for HCS12(X) Microcontrollers (Classic IDE) v5.1</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-we-set-up-a-64-bit-Integer-operations-under-CodeWarrior/m-p/404643#M11048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Xiumin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you create project , please try configure :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53025i0A3532C11ACE723A/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Sep 2015 01:34:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-we-set-up-a-64-bit-Integer-operations-under-CodeWarrior/m-p/404643#M11048</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-09-02T01:34:30Z</dc:date>
    </item>
    <item>
      <title>Re: How can we set up a 64 - bit Integer operations under  CodeWarrior Development Studio for HCS12(X) Microcontrollers (Classic IDE) v5.1</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-we-set-up-a-64-bit-Integer-operations-under-CodeWarrior/m-p/404644#M11049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Alice，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;        Thanks for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;         I've tried this, but it's floating point type, and use an integer that needs to change.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Sep 2015 01:46:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-we-set-up-a-64-bit-Integer-operations-under-CodeWarrior/m-p/404644#M11049</guid>
      <dc:creator>xiuminsong</dc:creator>
      <dc:date>2015-09-02T01:46:00Z</dc:date>
    </item>
    <item>
      <title>Re: How can we set up a 64 - bit Integer operations under  CodeWarrior Development Studio for HCS12(X) Microcontrollers (Classic IDE) v5.1</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-we-set-up-a-64-bit-Integer-operations-under-CodeWarrior/m-p/404645#M11050</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Xiumin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry&amp;nbsp; i said before is wrong .&lt;/P&gt;&lt;P&gt;the HCS12(x) chips is 16 bit , so the maximum bit is 32 , it can not&amp;nbsp; realize 64 bits.&lt;/P&gt;&lt;P&gt;For the kinetis chip , for it is 32 bit , so the longlong type is 64 bits.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Sep 2015 03:16:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-we-set-up-a-64-bit-Integer-operations-under-CodeWarrior/m-p/404645#M11050</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-09-08T03:16:25Z</dc:date>
    </item>
    <item>
      <title>Re: How can we set up a 64 - bit Integer operations under  CodeWarrior Development Studio for HCS12(X) Microcontrollers (Classic IDE) v5.1</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-we-set-up-a-64-bit-Integer-operations-under-CodeWarrior/m-p/404646#M11051</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Alice，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;      Thank you very much！&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Sep 2015 03:39:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-we-set-up-a-64-bit-Integer-operations-under-CodeWarrior/m-p/404646#M11051</guid>
      <dc:creator>xiuminsong</dc:creator>
      <dc:date>2015-09-08T03:39:17Z</dc:date>
    </item>
    <item>
      <title>Re: How can we set up a 64 - bit Integer operations under  CodeWarrior Development Studio for HCS12(X) Microcontrollers (Classic IDE) v5.1</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-we-set-up-a-64-bit-Integer-operations-under-CodeWarrior/m-p/404647#M11052</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's not true that 16bit MCU can't have 64bit integers in C. Even 8bit MCU's can do. But CW for S12(X) doesn't support it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Sep 2015 08:11:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-can-we-set-up-a-64-bit-Integer-operations-under-CodeWarrior/m-p/404647#M11052</guid>
      <dc:creator>kef2</dc:creator>
      <dc:date>2015-09-14T08:11:28Z</dc:date>
    </item>
  </channel>
</rss>