<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S12XE Periodic Interrupt Timer in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XE-Periodic-Interrupt-Timer/m-p/402792#M11013</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ray,&lt;/P&gt;&lt;P&gt;No, maximum is 8 channels.&lt;/P&gt;&lt;P&gt;Please look at Appendix D Derivative Differences in reference manual.&lt;/P&gt;&lt;P&gt;9S12XEP100, 9S12XEP768 have 8 channels PIT module.&lt;/P&gt;&lt;P&gt;Derivatives with lower amount of Flash has just four channel PIT module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Sep 2015 11:17:15 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2015-09-24T11:17:15Z</dc:date>
    <item>
      <title>S12XE Periodic Interrupt Timer</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XE-Periodic-Interrupt-Timer/m-p/402791#M11012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been looking at the datasheet for the S12XEP100 and I find there is two Periodic Interrupt Timers listed. These are,&lt;/P&gt;&lt;P&gt;S12PIT24B4CV2 (Four Timers)&lt;/P&gt;&lt;P&gt;S12PIT24B8CV2 (Eight Timers)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does this mean the are a total of twelve PIT timers ?. &lt;BR /&gt;If so I cannot find the output pins for the extra four.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If some S12XE only have four PIT timers, then I cannot find this information in the datasheet.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ray.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Sep 2015 09:01:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XE-Periodic-Interrupt-Timer/m-p/402791#M11012</guid>
      <dc:creator>rayhall</dc:creator>
      <dc:date>2015-09-24T09:01:01Z</dc:date>
    </item>
    <item>
      <title>Re: S12XE Periodic Interrupt Timer</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XE-Periodic-Interrupt-Timer/m-p/402792#M11013</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ray,&lt;/P&gt;&lt;P&gt;No, maximum is 8 channels.&lt;/P&gt;&lt;P&gt;Please look at Appendix D Derivative Differences in reference manual.&lt;/P&gt;&lt;P&gt;9S12XEP100, 9S12XEP768 have 8 channels PIT module.&lt;/P&gt;&lt;P&gt;Derivatives with lower amount of Flash has just four channel PIT module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Sep 2015 11:17:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XE-Periodic-Interrupt-Timer/m-p/402792#M11013</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2015-09-24T11:17:15Z</dc:date>
    </item>
  </channel>
</rss>