<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックSelf flash programming of S12DP512</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Self-flash-programming-of-S12DP512/m-p/401762#M11010</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;May I know can S12DP512 support self flash programming? E.g. Write data into the 512KBytes program memory.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 May 2015 09:23:31 GMT</pubDate>
    <dc:creator>monstor</dc:creator>
    <dc:date>2015-05-05T09:23:31Z</dc:date>
    <item>
      <title>Self flash programming of S12DP512</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Self-flash-programming-of-S12DP512/m-p/401762#M11010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;May I know can S12DP512 support self flash programming? E.g. Write data into the 512KBytes program memory.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 May 2015 09:23:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Self-flash-programming-of-S12DP512/m-p/401762#M11010</guid>
      <dc:creator>monstor</dc:creator>
      <dc:date>2015-05-05T09:23:31Z</dc:date>
    </item>
    <item>
      <title>Re: Self flash programming of S12DP512</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Self-flash-programming-of-S12DP512/m-p/401763#M11011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, that is possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to be able to program/erase all Flash without restriction, the program/erase function must be copied to and executed from a non-flash memory location, RAM or EEPROM for example.&lt;/P&gt;&lt;P&gt;A Flash block cannot be read whilst it is being programmed or erased. Therefore the program and erase function cannot be executed from the flash block which is being operated on. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the application note with the SW example for this specific subject:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2204.pdf"&gt;&lt;SPAN class="l"&gt;&lt;SPAN class="goog-trans-section l"&gt;Fast NVM Programming for the MC9S12DP256&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #afafaf;"&gt;&lt;A href="http://www.freescale.com/webapp/sps/download/license.jsp?colCode=AN2204SW&amp;amp;location=null"&gt;AN2204SW&lt;/A&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;iggi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 May 2015 08:51:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Self-flash-programming-of-S12DP512/m-p/401763#M11011</guid>
      <dc:creator>iggi</dc:creator>
      <dc:date>2015-05-13T08:51:24Z</dc:date>
    </item>
  </channel>
</rss>