<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Is Periodic Interrupt Timer and Enhanced Capture Timer both are different</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Is-Periodic-Interrupt-Timer-and-Enhanced-Capture-Timer-both-are/m-p/400876#M11005</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;if is different then how can I configure Periodic Interrupt Timer in processor expert for MC9S12XHZ512&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Jul 2015 16:10:12 GMT</pubDate>
    <dc:creator>kdn</dc:creator>
    <dc:date>2015-07-10T16:10:12Z</dc:date>
    <item>
      <title>Is Periodic Interrupt Timer and Enhanced Capture Timer both are different</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Is-Periodic-Interrupt-Timer-and-Enhanced-Capture-Timer-both-are/m-p/400876#M11005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;if is different then how can I configure Periodic Interrupt Timer in processor expert for MC9S12XHZ512&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jul 2015 16:10:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Is-Periodic-Interrupt-Timer-and-Enhanced-Capture-Timer-both-are/m-p/400876#M11005</guid>
      <dc:creator>kdn</dc:creator>
      <dc:date>2015-07-10T16:10:12Z</dc:date>
    </item>
    <item>
      <title>Re: Is Periodic Interrupt Timer and Enhanced Capture Timer both are different</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Is-Periodic-Interrupt-Timer-and-Enhanced-Capture-Timer-both-are/m-p/400877#M11006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;For periodic interrupts, you can use Periodic Interrupt Timer (PIT), Enhanced Capture Timer (ECT) or Real Time Interrupt (RTI, part of CRG module).&lt;/P&gt;&lt;P&gt;In attachment you can find simple example codes which generate periodic interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: Example code does not use PE.&lt;/P&gt;&lt;P&gt;Note: Example code was designed for S12XD family however behavior should be the same also for S12XHZ.&lt;/P&gt;&lt;P&gt;Note: Result periods will depend on frequency of your clock source.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jul 2015 11:35:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Is-Periodic-Interrupt-Timer-and-Enhanced-Capture-Timer-both-are/m-p/400877#M11006</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2015-07-13T11:35:26Z</dc:date>
    </item>
  </channel>
</rss>