<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: Rewrite the Pflash code on S12ZVM</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Rewrite-the-Pflash-code-on-S12ZVM/m-p/392034#M10911</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you!!&lt;/P&gt;&lt;P&gt;Ikki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 May 2015 12:43:42 GMT</pubDate>
    <dc:creator>ikkishingu</dc:creator>
    <dc:date>2015-05-15T12:43:42Z</dc:date>
    <item>
      <title>Rewrite the Pflash code on S12ZVM</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Rewrite-the-Pflash-code-on-S12ZVM/m-p/392032#M10909</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a question about S12ZVM Program Flash.&lt;/P&gt;&lt;P&gt;If the user wants to rewrite the Program Flash code by itself,&lt;/P&gt;&lt;P&gt;do the code(to rewrite Pflash) have to be executed on SRAM?&lt;/P&gt;&lt;P&gt;Or can it be executed on another Pflash region/sector(i.e. read-while-write)?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Ikki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Apr 2015 08:50:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Rewrite-the-Pflash-code-on-S12ZVM/m-p/392032#M10909</guid>
      <dc:creator>ikkishingu</dc:creator>
      <dc:date>2015-04-30T08:50:39Z</dc:date>
    </item>
    <item>
      <title>Re: Rewrite the Pflash code on S12ZVM</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Rewrite-the-Pflash-code-on-S12ZVM/m-p/392033#M10910</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Since there is only one Flash block on S12ZVM, the code must be executed from RAM.&lt;/P&gt;&lt;P&gt;It is not possible to access a Flash block while a code executes from the same. In case of two or more flash block, this would be possible - code executes on one and writes/read/erase the other block.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also some commands can be executed from EEPROM (the flash block on S12ZVM consist of P-Flash and EEPROM):&lt;/P&gt;&lt;P&gt;It is possible to read from P-Flash memory while some commands are executing on EEPROM memory.&lt;BR /&gt;It is not possible to read from EEPROM memory while a command is executing on P-Flash memory from the same block. &lt;BR /&gt;Simultaneous P-Flash and EEPROM operations are discussed in Flash Module (S12ZFTMRZ) chapter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;iggi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 May 2015 08:36:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Rewrite-the-Pflash-code-on-S12ZVM/m-p/392033#M10910</guid>
      <dc:creator>iggi</dc:creator>
      <dc:date>2015-05-13T08:36:23Z</dc:date>
    </item>
    <item>
      <title>Re: Rewrite the Pflash code on S12ZVM</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Rewrite-the-Pflash-code-on-S12ZVM/m-p/392034#M10911</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you!!&lt;/P&gt;&lt;P&gt;Ikki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 May 2015 12:43:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Rewrite-the-Pflash-code-on-S12ZVM/m-p/392034#M10911</guid>
      <dc:creator>ikkishingu</dc:creator>
      <dc:date>2015-05-15T12:43:42Z</dc:date>
    </item>
  </channel>
</rss>