<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I want to resolve MC9SS12ZVMC debugging problem. in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-want-to-resolve-MC9SS12ZVMC-debugging-problem/m-p/371325#M10713</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;maybe for MCU debugging purpose, it would be good to disconnect the MCU_RESET and BDM_RESET line from the TLE4263 regulator. &lt;/P&gt;&lt;P&gt;Keep the pull-up resistor on /RESET pin of MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also prior to that, you can try and add a 470nF cap (do not use &amp;gt;=1uF) between /RESET pin and GND for programming ONLY. A good solution would be if it is possible to add/remove the capacitor on the fly (as for some debugging you also want the resets from regulator to work).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope the info is helpful.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Apr 2015 10:52:15 GMT</pubDate>
    <dc:creator>iggi</dc:creator>
    <dc:date>2015-04-03T10:52:15Z</dc:date>
    <item>
      <title>I want to resolve MC9SS12ZVMC debugging problem.</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-want-to-resolve-MC9SS12ZVMC-debugging-problem/m-p/371324#M10712</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm using MC9SS12ZVMC128MKH(MCU) and TLE4263GMMC3(regulator).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now, there is problem about reset.&lt;/P&gt;&lt;P&gt;I try debug but can't debug because regulator's Reset.&lt;/P&gt;&lt;P&gt;So, I want to resolve Debugging Reset problem.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120256iC03C78284531915E/image-size/large?v=v2&amp;amp;px=999" title="21703_21703.jpg" alt="21703_21703.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/50088i5CC32BB7D69CD884/image-size/large?v=v2&amp;amp;px=999" title="regulator.JPG.jpg" alt="regulator.JPG.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120257iD71C104F8554948B/image-size/large?v=v2&amp;amp;px=999" title="21708_21708.jpg" alt="21708_21708.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20256i1342CE7A17C4C281/image-size/large?v=v2&amp;amp;px=999" title="mcu.JPG.jpg" alt="mcu.JPG.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120258iCC526CB77B00C516/image-size/large?v=v2&amp;amp;px=999" title="21709_21709.jpg" alt="21709_21709.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/50296i31C4D79A93EC117E/image-size/large?v=v2&amp;amp;px=999" title="bdm.JPG.jpg" alt="bdm.JPG.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Apr 2015 01:15:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-want-to-resolve-MC9SS12ZVMC-debugging-problem/m-p/371324#M10712</guid>
      <dc:creator>yoongonkim</dc:creator>
      <dc:date>2015-04-02T01:15:21Z</dc:date>
    </item>
    <item>
      <title>Re: I want to resolve MC9SS12ZVMC debugging problem.</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-want-to-resolve-MC9SS12ZVMC-debugging-problem/m-p/371325#M10713</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;maybe for MCU debugging purpose, it would be good to disconnect the MCU_RESET and BDM_RESET line from the TLE4263 regulator. &lt;/P&gt;&lt;P&gt;Keep the pull-up resistor on /RESET pin of MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also prior to that, you can try and add a 470nF cap (do not use &amp;gt;=1uF) between /RESET pin and GND for programming ONLY. A good solution would be if it is possible to add/remove the capacitor on the fly (as for some debugging you also want the resets from regulator to work).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope the info is helpful.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Apr 2015 10:52:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-want-to-resolve-MC9SS12ZVMC-debugging-problem/m-p/371325#M10713</guid>
      <dc:creator>iggi</dc:creator>
      <dc:date>2015-04-03T10:52:15Z</dc:date>
    </item>
  </channel>
</rss>