<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 How to interface a display 240 x 64 with T6963 using MC9s12xdp512?</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-interface-a-display-240-x-64-with-T6963-using/m-p/370830#M10699</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="hps"&gt;Need to&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;develop a project with&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;a display&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;240&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;x&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;64&lt;/SPAN&gt; &lt;SPAN class="atn hps"&gt;(&lt;/SPAN&gt;T6963) &lt;SPAN class="hps"&gt;and&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;I use&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;MC9s12XDP512&lt;/SPAN&gt;. &lt;/P&gt;&lt;P&gt;&lt;SPAN class="hps"&gt;Is there any&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;library&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;to control&lt;/SPAN&gt;? &lt;/P&gt;&lt;P&gt;&lt;SPAN class="hps"&gt;Thank you&lt;/SPAN&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 31 Oct 2014 18:05:18 GMT</pubDate>
    <dc:creator>sergioloncan</dc:creator>
    <dc:date>2014-10-31T18:05:18Z</dc:date>
    <item>
      <title>How to interface a display 240 x 64 with T6963 using MC9s12xdp512?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-interface-a-display-240-x-64-with-T6963-using/m-p/370830#M10699</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="hps"&gt;Need to&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;develop a project with&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;a display&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;240&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;x&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;64&lt;/SPAN&gt; &lt;SPAN class="atn hps"&gt;(&lt;/SPAN&gt;T6963) &lt;SPAN class="hps"&gt;and&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;I use&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;MC9s12XDP512&lt;/SPAN&gt;. &lt;/P&gt;&lt;P&gt;&lt;SPAN class="hps"&gt;Is there any&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;library&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;to control&lt;/SPAN&gt;? &lt;/P&gt;&lt;P&gt;&lt;SPAN class="hps"&gt;Thank you&lt;/SPAN&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Oct 2014 18:05:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-interface-a-display-240-x-64-with-T6963-using/m-p/370830#M10699</guid>
      <dc:creator>sergioloncan</dc:creator>
      <dc:date>2014-10-31T18:05:18Z</dc:date>
    </item>
    <item>
      <title>Re: How to interface a display 240 x 64 with T6963 using MC9s12xdp512?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-interface-a-display-240-x-64-with-T6963-using/m-p/370831#M10700</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can use any free port on the MCU, for example Port B, to connect 8x data lines D0-D7. Then you would need another port to connect control lines such as chip enable, R/W select etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyway, here is an older post which should be of interest. Please, check all the links, especially the one in the last response.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/53609"&gt;LCD Lib for MC9S08dz60 and T6963c&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;iggi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Nov 2014 10:12:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-interface-a-display-240-x-64-with-T6963-using/m-p/370831#M10700</guid>
      <dc:creator>iggi</dc:creator>
      <dc:date>2014-11-12T10:12:14Z</dc:date>
    </item>
  </channel>
</rss>