<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MM912J637 - Operation at 3.3Volts in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM912J637-Operation-at-3-3Volts/m-p/348748#M10553</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Hello Ian,&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;It will be possible to set VDDRX through an external regulator. The drawback is that you will have to handle the power supply and synchronization constraint by your own.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;The power management scheme (while connecting VDDX to VDDRX, and VDDH to VDDD2D, and RESET to RESETA) is insuring that at power up/down and after wake-up and entering into low power mode the device supplies are well set. This will require to be handled by the system of the user. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Also you need to take into account the Absolute Maximum Ratings and Operating Conditions of VDDRX as described in the datasheet.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;iggi&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Sep 2014 12:24:44 GMT</pubDate>
    <dc:creator>iggi</dc:creator>
    <dc:date>2014-09-05T12:24:44Z</dc:date>
    <item>
      <title>MM912J637 - Operation at 3.3Volts</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM912J637-Operation-at-3-3Volts/m-p/348747#M10552</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The MM912J637 (and MM912I637) data sheet states that operating conditions for VDDRX can range from 3.13 to 5.5 volts.&amp;nbsp; This seems clear enough.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Can I run the device from an external 3.3V regulator rather than looping VDDX to VDDRX?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Will there be a problem due to the Clamp5V supply during STOP mode?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The data sheets says for the VDDRX pin "This pin must be connected to VDDX.".&amp;nbsp; This suggests I can't do what I want to do. Also the low voltage interrupt and reset conditions mentioned in Section 3.5.2 (table 24) suggest it is pretty marginal.&amp;nbsp; So which data is correct.&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(I was going to use the VDDX output to shutoff the external 3.3V regulator during sleep/stop modes.)&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A couple of related things:&lt;/P&gt;&lt;P&gt;Section 3.3 Operating Conditions of the data sheet mentions that the range of operation for VDDRX is 3.13 to 5.5V.&amp;nbsp; Yet the 5V regulator output, VDDX, can range from 3.15 to 5.9V.&amp;nbsp; So the VDDX can possibly generate a voltage beyond the stated operating limits of the VDDRX input.&amp;nbsp; The data sheet says these can (maybe even normally are) connected together.&amp;nbsp; So why is the regulator output able to generate a voltage beyond the operating conditions?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The stated output voltage range of the VDDX regulator is enormous - 3.13 to 5.9V.&amp;nbsp; Why so large?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Aug 2014 06:19:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM912J637-Operation-at-3-3Volts/m-p/348747#M10552</guid>
      <dc:creator>igw</dc:creator>
      <dc:date>2014-08-11T06:19:27Z</dc:date>
    </item>
    <item>
      <title>Re: MM912J637 - Operation at 3.3Volts</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM912J637-Operation-at-3-3Volts/m-p/348748#M10553</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Hello Ian,&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;It will be possible to set VDDRX through an external regulator. The drawback is that you will have to handle the power supply and synchronization constraint by your own.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;The power management scheme (while connecting VDDX to VDDRX, and VDDH to VDDD2D, and RESET to RESETA) is insuring that at power up/down and after wake-up and entering into low power mode the device supplies are well set. This will require to be handled by the system of the user. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Also you need to take into account the Absolute Maximum Ratings and Operating Conditions of VDDRX as described in the datasheet.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;iggi&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Sep 2014 12:24:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM912J637-Operation-at-3-3Volts/m-p/348748#M10553</guid>
      <dc:creator>iggi</dc:creator>
      <dc:date>2014-09-05T12:24:44Z</dc:date>
    </item>
  </channel>
</rss>