<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollersのトピックabout the maximum allowed continuous current of S12ZVL</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/about-the-maximum-allowed-continuous-current-of-S12ZVL/m-p/340899#M10501</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In S12ZVL Reference Manual,&lt;/P&gt;&lt;P&gt;Maximum allowed continuous current on PP1, PP3 and PP5 is specified -20 ~ 10mA as I_EVDD.&lt;/P&gt;&lt;P&gt;Which understanding is correct about this I_EVDD?&lt;/P&gt;&lt;P&gt; - I_EVDD is the spec for each port&lt;/P&gt;&lt;P&gt; or&lt;/P&gt;&lt;P&gt; - I_EVDD is the spec of the current sum of PP1, PP3 and PP5&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Sep 2014 06:25:09 GMT</pubDate>
    <dc:creator>ikkishingu</dc:creator>
    <dc:date>2014-09-24T06:25:09Z</dc:date>
    <item>
      <title>about the maximum allowed continuous current of S12ZVL</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/about-the-maximum-allowed-continuous-current-of-S12ZVL/m-p/340899#M10501</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In S12ZVL Reference Manual,&lt;/P&gt;&lt;P&gt;Maximum allowed continuous current on PP1, PP3 and PP5 is specified -20 ~ 10mA as I_EVDD.&lt;/P&gt;&lt;P&gt;Which understanding is correct about this I_EVDD?&lt;/P&gt;&lt;P&gt; - I_EVDD is the spec for each port&lt;/P&gt;&lt;P&gt; or&lt;/P&gt;&lt;P&gt; - I_EVDD is the spec of the current sum of PP1, PP3 and PP5&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Sep 2014 06:25:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/about-the-maximum-allowed-continuous-current-of-S12ZVL/m-p/340899#M10501</guid>
      <dc:creator>ikkishingu</dc:creator>
      <dc:date>2014-09-24T06:25:09Z</dc:date>
    </item>
    <item>
      <title>Re: about the maximum allowed continuous current of S12ZVL</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/about-the-maximum-allowed-continuous-current-of-S12ZVL/m-p/340900#M10502</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The S12ZVL Reference Manual has not yet been released, so it is not clear exactly which information you are referring to.&lt;/P&gt;&lt;P&gt;However to clarify a few points.&lt;/P&gt;&lt;P&gt;PP1, PP3 and PP5 are not EVDD pins. PP1, PP3 and PP5 have increased current driving capability to VSSX ground.&lt;/P&gt;&lt;P&gt;PP7 is the EVDD1 pin which has increased current driving capability to VDDX.&lt;/P&gt;&lt;P&gt;The EVDD1 specification has a range of -20mA to +10mA for that pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The PP1,PP3 and PP5 spec. maximum is +25mA for each pin.&lt;/P&gt;&lt;P&gt;The total maximum current of 80mA (absolute maximum ratings) must also be taken into consideration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The first official reference manual shall be published soon.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DPB&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Sep 2014 11:44:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/about-the-maximum-allowed-continuous-current-of-S12ZVL/m-p/340900#M10502</guid>
      <dc:creator>DPB</dc:creator>
      <dc:date>2014-09-24T11:44:29Z</dc:date>
    </item>
    <item>
      <title>Re: about the maximum allowed continuous current of S12ZVL</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/about-the-maximum-allowed-continuous-current-of-S12ZVL/m-p/340901#M10503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;DPB-san,&lt;/P&gt;&lt;P&gt;Thank you for your helpful information.&lt;/P&gt;&lt;P&gt;It makes sense to me. I can understand clearly!!&lt;/P&gt;&lt;P&gt;Ikki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Sep 2014 06:50:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/about-the-maximum-allowed-continuous-current-of-S12ZVL/m-p/340901#M10503</guid>
      <dc:creator>ikkishingu</dc:creator>
      <dc:date>2014-09-25T06:50:52Z</dc:date>
    </item>
  </channel>
</rss>