<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Several Questions for S12ZVM in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Several-Questions-for-S12ZVM/m-p/339335#M10492</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q1. Is it posible to measure Vreg or Bootstrap voltage?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Q2. Is there any references for temperature calibration?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Q3. In freemaster, scaling values are different each other when convert from frac16 to real value, reason why?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (e.g. Actual Speed RPM is converted with 17895, DCBusCurrentZC is converted with 32767, DC Bus voltage is converted with 13653)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Q4. the values in ADC Result list array are over 2^12, reason why?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Oct 2014 11:06:43 GMT</pubDate>
    <dc:creator>young-kyunpark</dc:creator>
    <dc:date>2014-10-21T11:06:43Z</dc:date>
    <item>
      <title>Several Questions for S12ZVM</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Several-Questions-for-S12ZVM/m-p/339335#M10492</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q1. Is it posible to measure Vreg or Bootstrap voltage?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Q2. Is there any references for temperature calibration?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Q3. In freemaster, scaling values are different each other when convert from frac16 to real value, reason why?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (e.g. Actual Speed RPM is converted with 17895, DCBusCurrentZC is converted with 32767, DC Bus voltage is converted with 13653)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Q4. the values in ADC Result list array are over 2^12, reason why?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Oct 2014 11:06:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Several-Questions-for-S12ZVM/m-p/339335#M10492</guid>
      <dc:creator>young-kyunpark</dc:creator>
      <dc:date>2014-10-21T11:06:43Z</dc:date>
    </item>
    <item>
      <title>Re: Several Questions for S12ZVM</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Several-Questions-for-S12ZVM/m-p/339336#M10493</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q1 reply: &lt;/P&gt;&lt;P&gt;ADC0 internal_4 channel is mapped to the BATS monitor, which is a 1:9 scaled down VSUP. &lt;/P&gt;&lt;P&gt;To measure this it is also necessary to set BSUAE and BSUSE in the BATE register.&lt;/P&gt;&lt;P&gt;ADC0 internal_1 can also be mapped to the VREG bandgap voltage.&lt;/P&gt;&lt;P&gt;ADC0 and ADC1 channels internal_3 are mapped to the 1:5 scaled GDU DC link voltage (HD).&lt;/P&gt;&lt;P&gt;The bootstrap voltage cannot be directly measured on chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q2 reply:&lt;/P&gt;&lt;P&gt;Calibration must be done by the user&lt;/P&gt;&lt;P&gt;The application note AN3624 which was written for S12X still basically applies for S12Z.&lt;/P&gt;&lt;P&gt;The temperature sensors are mapped to the ADC channels as shown in RM Table 1-7 and 1-8.&lt;/P&gt;&lt;P&gt;The temperature slope is given in Table B-1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q3: I am not a freemaster expert, so can't comment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q4 reply:&lt;/P&gt;&lt;P&gt;By default the 12-bit values are left justified in a 16-bit field.&lt;/P&gt;&lt;P&gt;They can be configured as right-justified by the DJM bit.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Oct 2014 08:31:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Several-Questions-for-S12ZVM/m-p/339336#M10493</guid>
      <dc:creator>DPB</dc:creator>
      <dc:date>2014-10-23T08:31:31Z</dc:date>
    </item>
  </channel>
</rss>