<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: CAN code</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CAN-code/m-p/330782#M10442</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, from that portion of code it is not possible to find out why it's not working.&lt;/P&gt;&lt;P&gt;The most probably CAN initializtion is not correctly done, or maybe (Tx/Rx) interrupts have no definition.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the link below you can download S12X pack of example in which two are for the CAN. You can use that as a reference:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95116"&gt;S12X Examples Pack&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;iggi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Jan 2015 13:56:18 GMT</pubDate>
    <dc:creator>iggi</dc:creator>
    <dc:date>2015-01-07T13:56:18Z</dc:date>
    <item>
      <title>CAN code</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CAN-code/m-p/330781#M10441</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MY CAN code is not working , anyone have any idea &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CAN1TIER = 0x07;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;//CAN1TFLG =CAN1TFLG_TXE0_MASK;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; CAN1TFLG = 0x01;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CAN1TXTBPR = 0x01;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CAN1TXDLR = 0x08;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CAN1TXIDR3 = 0x00;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CAN1TXIDR2 = 0x00;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CAN1TXIDR1 = 0x00;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CAN1TXIDR0 = 0xFF;&amp;nbsp;&amp;nbsp;&amp;nbsp; //SID&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CAN1TXDSR0 = 0xFF;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //DATA&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CAN1TXDSR1 = 0xFF;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CAN1TXDSR2 = 0xFF;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CAN1TXDSR3 = 0x00;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CAN1TXDSR4 = 0x00;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CAN1TXDSR5 = 0x00;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CAN1TXDSR6 = 0x00;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CAN1TXDSR7 = 0x00;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 07 Dec 2014 19:07:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CAN-code/m-p/330781#M10441</guid>
      <dc:creator>kdn</dc:creator>
      <dc:date>2014-12-07T19:07:01Z</dc:date>
    </item>
    <item>
      <title>Re: CAN code</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CAN-code/m-p/330782#M10442</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, from that portion of code it is not possible to find out why it's not working.&lt;/P&gt;&lt;P&gt;The most probably CAN initializtion is not correctly done, or maybe (Tx/Rx) interrupts have no definition.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the link below you can download S12X pack of example in which two are for the CAN. You can use that as a reference:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95116"&gt;S12X Examples Pack&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;iggi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jan 2015 13:56:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CAN-code/m-p/330782#M10442</guid>
      <dc:creator>iggi</dc:creator>
      <dc:date>2015-01-07T13:56:18Z</dc:date>
    </item>
  </channel>
</rss>