<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: MC33812 / S12P Small Engine Control.</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC33812-S12P-Small-Engine-Control/m-p/327307#M10411</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Franceso,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SW included in the CD is ready to use. It is already configured for S12P. You can fidn the rouines in the Low_Level subfolder which is Sources folder of the SW Example project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here are some links to smilar topics on the community that can be of help:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/335682"&gt;Re: Help, NEW to Codewarrior IDE S12 V5.0 and KIT33812ECUEVME&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/message/334386"&gt;Re: KIT33812ECUEVME&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;iggi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Nov 2014 11:17:11 GMT</pubDate>
    <dc:creator>iggi</dc:creator>
    <dc:date>2014-11-20T11:17:11Z</dc:date>
    <item>
      <title>MC33812 / S12P Small Engine Control.</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC33812-S12P-Small-Engine-Control/m-p/327306#M10410</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi, I bought the kit reference design - MC33812 / S12P Small Engine Control. I wanted to ask if the sample software in the CD is ready to use or you need to change. The simulation runs with debugging, but there are no signs of spark and fuel injection. In addition, the routines spi, sci and mc33812perchè they are not prepared for the micro mc9s12p? thanks for any clarification&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Nov 2014 11:25:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC33812-S12P-Small-Engine-Control/m-p/327306#M10410</guid>
      <dc:creator>francescodisilv</dc:creator>
      <dc:date>2014-11-10T11:25:30Z</dc:date>
    </item>
    <item>
      <title>Re: MC33812 / S12P Small Engine Control.</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC33812-S12P-Small-Engine-Control/m-p/327307#M10411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Franceso,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SW included in the CD is ready to use. It is already configured for S12P. You can fidn the rouines in the Low_Level subfolder which is Sources folder of the SW Example project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here are some links to smilar topics on the community that can be of help:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/335682"&gt;Re: Help, NEW to Codewarrior IDE S12 V5.0 and KIT33812ECUEVME&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/message/334386"&gt;Re: KIT33812ECUEVME&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;iggi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Nov 2014 11:17:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC33812-S12P-Small-Engine-Control/m-p/327307#M10411</guid>
      <dc:creator>iggi</dc:creator>
      <dc:date>2014-11-20T11:17:11Z</dc:date>
    </item>
  </channel>
</rss>