<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic I need a sample schematic using the MC9S12DT128. My circuit I designed isn't working. in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-need-a-sample-schematic-using-the-MC9S12DT128-My-circuit-I/m-p/314737#M10355</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I designed a circuit around the MC9S12DT128BMPV. I'm using an external 16MHz clock. When I power up there are some erratic square wave signals on the I/O pins. It seems like it is going through some type of continuous reset. I have the reset line pulled high with a 5K resistor. CW with a Cyclone can't communicate. Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 01 Jul 2014 20:04:56 GMT</pubDate>
    <dc:creator>gerryhermann</dc:creator>
    <dc:date>2014-07-01T20:04:56Z</dc:date>
    <item>
      <title>I need a sample schematic using the MC9S12DT128. My circuit I designed isn't working.</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-need-a-sample-schematic-using-the-MC9S12DT128-My-circuit-I/m-p/314737#M10355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I designed a circuit around the MC9S12DT128BMPV. I'm using an external 16MHz clock. When I power up there are some erratic square wave signals on the I/O pins. It seems like it is going through some type of continuous reset. I have the reset line pulled high with a 5K resistor. CW with a Cyclone can't communicate. Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Jul 2014 20:04:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-need-a-sample-schematic-using-the-MC9S12DT128-My-circuit-I/m-p/314737#M10355</guid>
      <dc:creator>gerryhermann</dc:creator>
      <dc:date>2014-07-01T20:04:56Z</dc:date>
    </item>
    <item>
      <title>Re: I need a sample schematic using the MC9S12DT128. My circuit I designed isn't working.</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-need-a-sample-schematic-using-the-MC9S12DT128-My-circuit-I/m-p/314738#M10356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gerry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to recommend you an app note, the AN2727 Designing Hardware for the HCS12 D-Family:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2727.pdf"&gt;cache.freescale.com/files/microcontrollers/doc/app_note/AN2727.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly go through it and check if you have anything different than stated in the app note such as:&lt;/P&gt;&lt;P&gt;- Power supply connections&lt;/P&gt;&lt;P&gt;- Control pin connections&lt;/P&gt;&lt;P&gt;- Oscillator options&lt;/P&gt;&lt;P&gt;etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;iggi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jul 2014 13:01:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-need-a-sample-schematic-using-the-MC9S12DT128-My-circuit-I/m-p/314738#M10356</guid>
      <dc:creator>iggi</dc:creator>
      <dc:date>2014-07-09T13:01:19Z</dc:date>
    </item>
  </channel>
</rss>